FittingOverstockBuilderTypes Enumeration¶
NXOpen.Routing.FittingOverstockBuilder.Types is an alias for NXOpen.Routing.FittingOverstockBuilderTypes
-
class
NXOpen.Routing.
FittingOverstockBuilderTypes
¶ Bases:
object
Overstock application method. This defines the way in which to apply the overstock on faces of the routing parts.
Enum Members
Enum Member Enum Member Description EntirePart Entire Part EntireFace Entire Face PartialFace Partial Face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-