AssignTangencyBuilder Class¶
-
class
NXOpen.Routing.
AssignTangencyBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Routing.AssignTangencyBuilder
object.Provides support for
NXOpen.Routing.SplinePathBuilder
when assigning tangency constraints between adjacent splines.To create a new instance of this class, use
NXOpen.Routing.SplinePathBuilder.CreateAssignTangencyBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
AssignTangencySide | Returns or sets the tangency side NXOpen.Routing.AssignTangencyBuilder.TangencySide to assign tangency |
SelectedTangencyGroup | Returns or sets the selected NXOpen.Routing.TangencyGroupBuilder to assign tangency at specified side of the spline. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AssignTangency | Assign tangency at specified side of the spline. |
AssignTangencyAtPort | Assign tangency at attached port. |
Commit | Commits any edits that have been applied to the builder. |
CreateTangencyGroupBuilder | Creates a NXOpen.Routing.TangencyGroupBuilder object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemoveTangency | Remove tangency at specified side of the spline. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AssignTangencyBuilderTangencySide Enumeration | Describes which side of the spline to assign tangency. |
Property Detail¶
AssignTangencySide¶
-
AssignTangencyBuilder.
AssignTangencySide
¶ Returns or sets the tangency side
NXOpen.Routing.AssignTangencyBuilder.TangencySide
to assign tangency-------------------------------------
Getter Method
Signature
AssignTangencySide
Returns: Return type: NXOpen.Routing.AssignTangencyBuilderTangencySide
New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
AssignTangencySide
Parameters: tangencySide ( NXOpen.Routing.AssignTangencyBuilderTangencySide
) –New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
SelectedTangencyGroup¶
-
AssignTangencyBuilder.
SelectedTangencyGroup
¶ Returns or sets the selected
NXOpen.Routing.TangencyGroupBuilder
to assign tangency at specified side of the spline.-------------------------------------
Getter Method
Signature
SelectedTangencyGroup
Returns: Return type: NXOpen.Routing.TangencyGroupBuilder
New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
-------------------------------------
Setter Method
Signature
SelectedTangencyGroup
Parameters: selectedTangencyGroup ( NXOpen.Routing.TangencyGroupBuilder
) –New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
Method Detail¶
AssignTangency¶
-
AssignTangencyBuilder.
AssignTangency
¶ Assign tangency at specified side of the spline.
See
NXOpen.Routing.AssignTangencyBuilderTangencySide
for valid options.Signature
AssignTangency(segments, tangencySide)
Parameters: - segments (list of
NXOpen.Curve
) – - tangencySide (
NXOpen.Routing.AssignTangencyBuilderTangencySide
) –
New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
- segments (list of
AssignTangencyAtPort¶
-
AssignTangencyBuilder.
AssignTangencyAtPort
¶ Assign tangency at attached port.
See
NXOpen.Routing.AssignTangencyBuilderTangencySide
for valid options.Signature
AssignTangencyAtPort(tangencySide)
Parameters: tangencySide ( NXOpen.Routing.AssignTangencyBuilderTangencySide
) –New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
CreateTangencyGroupBuilder¶
-
AssignTangencyBuilder.
CreateTangencyGroupBuilder
¶ Creates a
NXOpen.Routing.TangencyGroupBuilder
object.Signature
CreateTangencyGroupBuilder()
Returns: Return type: NXOpen.Routing.TangencyGroupBuilder
New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
RemoveTangency¶
-
AssignTangencyBuilder.
RemoveTangency
¶ Remove tangency at specified side of the spline.
See
NXOpen.Routing.AssignTangencyBuilderTangencySide
for valid options.Signature
RemoveTangency(tangencySide)
Parameters: tangencySide ( NXOpen.Routing.AssignTangencyBuilderTangencySide
) –New in version NX12.0.0.
License requirements: routing_base (“Routing Basic”)
Validate¶
-
AssignTangencyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.