AssignTangencyBuilderTangencySide Enumeration¶
NXOpen.Routing.AssignTangencyBuilder.TangencySide is an alias for NXOpen.Routing.AssignTangencyBuilderTangencySide
-
class
NXOpen.Routing.
AssignTangencyBuilderTangencySide
¶ Bases:
object
Describes which side of the spline to assign tangency.
Enum Members
Enum Member Enum Member Description Undefined The tangency side is undefined. Source Assign tangency at source ControlPoint. Target Assign tangency at target ControlPoint. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-