EnumerationArgument Class¶
-
class
NXOpen.Report.
EnumerationArgument
¶ Bases:
NXOpen.Report.BaseArgument
Represents an argument for enumeration type data.
Not support KF.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
DefaultValue | Returns or sets the argument default value. |
DisplayName | Returns or sets the argument display name |
Hint | Returns or sets the argument hint. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
Optional | Returns or sets a value that indicates whether this argument is optional or not. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetEnumerationOptions | Gets the enumeration options. |
Prints a representation of this object to the system log file. | |
SetEnumerationOptions | Sets the enumeration options. |
SetName | Sets the custom name of the object. |
Property Detail¶
DefaultValue¶
-
EnumerationArgument.
DefaultValue
¶ Returns or sets the argument default value.
The default value index is between 0 and options count queried by
NXOpen.Report.EnumerationArgument.GetEnumerationOptions()
, 0 is inclusive.-------------------------------------
Getter Method
Signature
DefaultValue
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefaultValue
Parameters: defaultValueIndex (int) – New in version NX11.0.0.
License requirements: None.
IsOccurrence¶
-
EnumerationArgument.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
EnumerationArgument.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
EnumerationArgument.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
EnumerationArgument.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
EnumerationArgument.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
EnumerationArgument.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
EnumerationArgument.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetEnumerationOptions¶
-
EnumerationArgument.
GetEnumerationOptions
¶ Gets the enumeration options.
Signature
GetEnumerationOptions()
Returns: Return type: list of str New in version NX11.0.0.
License requirements: None.
Print¶
-
EnumerationArgument.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetEnumerationOptions¶
-
EnumerationArgument.
SetEnumerationOptions
¶ Sets the enumeration options.
Signature
SetEnumerationOptions(enumerationOptions)
Parameters: enumerationOptions (list of str) – New in version NX11.0.0.
License requirements: None.
SetName¶
-
EnumerationArgument.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.