CushionControl Class

Properties

Property Description
IsOccurrence Returns whether this object is an occurrence or not.
JournalIdentifier Returns the identifier that would be recorded in a journal for this object.
Name Returns the custom name of the object.
OwningComponent Returns the owning component, if this object is an occurrence.
OwningPart Returns the owning part of this object
Prototype Returns the prototype of this object if it is an occurrence.
Tag Returns the Tag for this object.

Methods

Method Description
CreateAttributeIterator Create an attribute iterator
DeleteAllAttributesByType Deletes all attributes of a specific type.
DeleteAttributeByTypeAndTitle Deletes an attribute by type and title.
DeleteUserAttribute Deletes the first attribute encountered with the given Type, Title.
DeleteUserAttributes Deletes the attributes on the object, if any, that satisfy the given iterator
FindObject Finds the NXOpen.NXObject with the given identifier as recorded in a journal.
GetAttributeTitlesByType Gets all the attribute titles of a specific type.
GetBooleanUserAttribute Gets a boolean attribute by Title and array Index.
GetComputationalTimeUserAttribute Gets a time attribute by Title and array Index.
GetIntegerAttribute Gets an integer attribute by title.
GetIntegerUserAttribute Gets an integer attribute by Title and array Index.
GetNextUserAttribute Gets the next attribute encountered on the object, if any, that satisfies the given iterator.
GetPdmReferenceAttributeValue Gets the value of PDM Reference attribute for given object.
GetRealAttribute Gets a real attribute by title.
GetRealUserAttribute Gets a real attribute by Title and array Index.
GetReferenceAttribute Gets the reference string (not the calculated value) of a string attribute that uses a reference string.
GetStringAttribute Gets a string attribute value by title.
GetStringUserAttribute Gets a string attribute by Title and array Index.
GetTimeAttribute Gets a time attribute by title.
GetTimeUserAttribute Gets a time attribute by Title and array Index.
GetUserAttribute Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index.
GetUserAttributeAsString Gets the first attribute encountered on the object, if any, with a given title, type and array index.
GetUserAttributeCount Gets the count of set attributes on the object, if any, that satisfy the given iterator.
GetUserAttributeLock Determine the lock of the given attribute.
GetUserAttributeSize Gets the size of the first attribute encountered on the object, if any, with a given Title and Type.
GetUserAttributeSourceObjects Returns an array of objects from which this object presents attributes.
GetUserAttributes Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator.
GetUserAttributesAsStrings Gets all the attributes that have been set on the given object.
HasUserAttribute Determines if an attribute exists on the object, that satisfies the given iterator
Print Prints a representation of this object to the system log file.
SetAttribute Creates or modifies an integer attribute.
SetBooleanUserAttribute Creates or modifies a boolean attribute with the option to update or not.
SetName Sets the custom name of the object.
SetPdmReferenceAttribute Sets the value of PDM Reference attribute on the object.
SetReferenceAttribute Creates or modifies a string attribute which uses a reference string.
SetTimeAttribute Creates or modifies a time attribute.
SetTimeUserAttribute Creates or modifies a time attribute with the option to update or not.
SetUserAttribute Creates or modifies an attribute with the option to update or not.
SetUserAttributeLock Lock or unlock the given attribute.

Property Detail

IsOccurrence

JournalIdentifier

Name

OwningComponent

OwningPart

Prototype

Method Detail

FindObject

Print

SetName