ViewVisualizationVisualHiddenEdgesType Enumeration¶
NXOpen.Preferences.ViewVisualizationVisual.HiddenEdgesType is an alias for NXOpen.Preferences.ViewVisualizationVisualHiddenEdgesType
-
class
NXOpen.Preferences.
ViewVisualizationVisualHiddenEdgesType
¶ Bases:
object
Describes the available hidden edges types. Determines how hidden edges are displayed in the selected view.
Deprecated since version NX4.0.0: Use
NXOpen.Preferences.ViewVisualizationVisualHiddenEdges
instead.Enum Members
Enum Member Enum Member Description Visible All edges in a solid body that are hidden appear as solid lines Invisible grid line display of all existing and subsequently created solid bodies in the selected view, except that portions of geometry and text that appear behind solid bodies are erased Dashed grid line display of all existing and subsequently created solid bodies in the selected view, except that all portions of the geometry and text that appear behind solid bodies are displayed as dashed lines GrayThin All hidden edges in the color gray, with solid font and thin width. HiddenSurface Faceted display of all existing and subsequently created bodies in the selected view -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-