ViewVisualizationVisualHiddenEdges Enumeration

NXOpen.Preferences.ViewVisualizationVisual.HiddenEdges is an alias for NXOpen.Preferences.ViewVisualizationVisualHiddenEdges

class NXOpen.Preferences.ViewVisualizationVisualHiddenEdges

Bases: object

Describes the appearance of hidden edges displayed in the view.

Enum Members

Enum Member Enum Member Description
Visible
Invisible
GrayThin
Dashed
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.