SessionWorkPlane Class¶
-
class
NXOpen.Preferences.
SessionWorkPlane
¶ Bases:
object
Represents the set of WorkPlane preferences applicable to session
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX3.0.0.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.SessionVisualizationEmphasis
.
Properties¶
Property | Description |
---|---|
ObjectOffWorkPlane | Returns or sets the object off work plane. |
Methods¶
Enumerations¶
SessionWorkPlaneObjectDisplay Enumeration | Describes whether the object off work plane is normal display or dim and selectable or dim and non selectable |
Property Detail¶
ObjectOffWorkPlane¶
-
SessionWorkPlane.
ObjectOffWorkPlane
¶ Returns or sets the object off work plane.
Comes under Display tab. This preference is to de-emphasize or “dim” all objects in the work plane.
-------------------------------------
Getter Method
Signature
ObjectOffWorkPlane
Returns: Return type: NXOpen.Preferences.SessionWorkPlaneObjectDisplay
New in version NX3.0.0.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.SessionVisualizationEmphasis
.License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectOffWorkPlane
Parameters: objectOffWorkPlane ( NXOpen.Preferences.SessionWorkPlaneObjectDisplay
) –New in version NX3.0.0.
Deprecated since version NX8.5.0: See
NXOpen.Preferences.SessionVisualizationEmphasis
.License requirements: None.