SessionVisualizationEmphasis Class¶
-
class
NXOpen.Preferences.
SessionVisualizationEmphasis
¶ Bases:
object
Represents visualization preferences for emphasis that are applicable to the entire session.
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ObjectsOffSketchWorkPlaneNonSelectable | Returns or sets the setting that controls whether or not objects off the work plane are non-selectable in the Sketch Task Environment. |
ObjectsOffWcsWorkPlaneNonSelectable | Returns or sets the setting that controls whether or not objects off the WCS work plane are non-selectable. |
ProductInterfaceEmphasis | Returns or sets the setting that controls whether or not Product Interface objects are emphasized. |
SeeThruAll | Returns or sets the setting that controls whether or not all less important objects are de-emphasized. |
SeeThruDeEmphasizedObjects | Returns or sets the setting that controls whether or not See-Thru is applied to de-emphasized objects. |
SeeThruPreview | Returns or sets the setting that controls whether or not all less important objects are de-emphasized related to the Model Preview. |
SeeThruSection | Returns or sets the setting that controls whether or not geometry on the section plane is emphasized. |
SketchWorkPlaneEmphasis | Returns or sets the setting that controls whether or not objects on the work plane are emphasized in the Sketch Task Environment. |
WcsWorkPlaneEmphasis | Returns or sets the setting that controls whether or not objects on the WCS work plane are emphasized. |
WorkPartEmphasis | Returns or sets the setting that controls whether or not the work part is emphasized. |
Methods¶
Property Detail¶
ObjectsOffSketchWorkPlaneNonSelectable¶
-
SessionVisualizationEmphasis.
ObjectsOffSketchWorkPlaneNonSelectable
¶ Returns or sets the setting that controls whether or not objects off the work plane are non-selectable in the Sketch Task Environment.
-------------------------------------
Getter Method
Signature
ObjectsOffSketchWorkPlaneNonSelectable
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectsOffSketchWorkPlaneNonSelectable
Parameters: objectsOffSketchWorkPlaneNonSelectable (bool) – New in version NX8.5.0.
License requirements: None.
ObjectsOffWcsWorkPlaneNonSelectable¶
-
SessionVisualizationEmphasis.
ObjectsOffWcsWorkPlaneNonSelectable
¶ Returns or sets the setting that controls whether or not objects off the WCS work plane are non-selectable.
-------------------------------------
Getter Method
Signature
ObjectsOffWcsWorkPlaneNonSelectable
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectsOffWcsWorkPlaneNonSelectable
Parameters: objectsOffWcsWorkPlaneNonSelectable (bool) – New in version NX8.5.0.
License requirements: None.
ProductInterfaceEmphasis¶
-
SessionVisualizationEmphasis.
ProductInterfaceEmphasis
¶ Returns or sets the setting that controls whether or not Product Interface objects are emphasized.
-------------------------------------
Getter Method
Signature
ProductInterfaceEmphasis
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProductInterfaceEmphasis
Parameters: productInterfaceEmphasis (bool) – New in version NX8.5.0.
License requirements: None.
SeeThruAll¶
-
SessionVisualizationEmphasis.
SeeThruAll
¶ Returns or sets the setting that controls whether or not all less important objects are de-emphasized.
-------------------------------------
Getter Method
Signature
SeeThruAll
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruAll
Parameters: seeThruAll (bool) – New in version NX8.5.0.
License requirements: None.
SeeThruDeEmphasizedObjects¶
-
SessionVisualizationEmphasis.
SeeThruDeEmphasizedObjects
¶ Returns or sets the setting that controls whether or not See-Thru is applied to de-emphasized objects.
-------------------------------------
Getter Method
Signature
SeeThruDeEmphasizedObjects
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruDeEmphasizedObjects
Parameters: seeThruDeEmphasizedObjects (bool) – New in version NX8.5.0.
License requirements: None.
SeeThruPreview¶
-
SessionVisualizationEmphasis.
SeeThruPreview
¶ Returns or sets the setting that controls whether or not all less important objects are de-emphasized related to the Model Preview.
-------------------------------------
Getter Method
Signature
SeeThruPreview
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruPreview
Parameters: seeThruPreview (bool) – New in version NX8.5.0.
License requirements: None.
SeeThruSection¶
-
SessionVisualizationEmphasis.
SeeThruSection
¶ Returns or sets the setting that controls whether or not geometry on the section plane is emphasized.
-------------------------------------
Getter Method
Signature
SeeThruSection
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeeThruSection
Parameters: seeThruSection (bool) – New in version NX8.5.0.
License requirements: None.
SketchWorkPlaneEmphasis¶
-
SessionVisualizationEmphasis.
SketchWorkPlaneEmphasis
¶ Returns or sets the setting that controls whether or not objects on the work plane are emphasized in the Sketch Task Environment.
-------------------------------------
Getter Method
Signature
SketchWorkPlaneEmphasis
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SketchWorkPlaneEmphasis
Parameters: sketchWorkPlaneEmphasis (bool) – New in version NX8.5.0.
License requirements: None.
WcsWorkPlaneEmphasis¶
-
SessionVisualizationEmphasis.
WcsWorkPlaneEmphasis
¶ Returns or sets the setting that controls whether or not objects on the WCS work plane are emphasized.
-------------------------------------
Getter Method
Signature
WcsWorkPlaneEmphasis
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WcsWorkPlaneEmphasis
Parameters: wcsWorkPlaneEmphasis (bool) – New in version NX8.5.0.
License requirements: None.
WorkPartEmphasis¶
-
SessionVisualizationEmphasis.
WorkPartEmphasis
¶ Returns or sets the setting that controls whether or not the work part is emphasized.
-------------------------------------
Getter Method
Signature
WorkPartEmphasis
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WorkPartEmphasis
Parameters: workPartEmphasis (bool) – New in version NX8.5.0.
License requirements: None.