SessionVisualizationHighEndRendering Class¶
-
class
NXOpen.Preferences.
SessionVisualizationHighEndRendering
¶ Bases:
object
Represents the set of visualization preferences under High End Rendering tab applicable to entire session
To obtain an instance of this class, refer to
NXOpen.Preferences.SessionPreferences
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
StudioMaterialEditorEditingMode | Returns or sets the Studio Material Editor editing mode |
Methods¶
Enumerations¶
SessionVisualizationHighEndRenderingMaterialEditorEditingMode Enumeration | The two Studio Material Editor editing modes |
Property Detail¶
StudioMaterialEditorEditingMode¶
-
SessionVisualizationHighEndRendering.
StudioMaterialEditorEditingMode
¶ Returns or sets the Studio Material Editor editing mode
-------------------------------------
Getter Method
Signature
StudioMaterialEditorEditingMode
Returns: Return type: NXOpen.Preferences.SessionVisualizationHighEndRenderingMaterialEditorEditingMode
New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StudioMaterialEditorEditingMode
Parameters: newMode ( NXOpen.Preferences.SessionVisualizationHighEndRenderingMaterialEditorEditingMode
) –New in version NX11.0.1.
License requirements: None.