SessionVisualizationHighEndRenderingMaterialEditorEditingMode Enumeration¶
NXOpen.Preferences.SessionVisualizationHighEndRendering.MaterialEditorEditingMode is an alias for NXOpen.Preferences.SessionVisualizationHighEndRenderingMaterialEditorEditingMode
-
class
NXOpen.Preferences.
SessionVisualizationHighEndRenderingMaterialEditorEditingMode
¶ Bases:
object
The two Studio Material Editor editing modes
Enum Members
Enum Member Enum Member Description Basic Studio Material Editor in Basic properties mode Full Studio Material Editor in Full properties mode -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-