RoutingMechanical Class¶
-
class
NXOpen.Preferences.
RoutingMechanical
¶ Bases:
object
The RoutingMechanical object stores a set of route mechanical preferences.
To obtain an instance of this class, refer to
NXOpen.Preferences.RoutingApplicationView
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
GetIsInitialized | Returns the information of whether the mechanical preferences section exists in the application view file. |
GetLineColorTypes | Returns types of string in line_color field. |
GetLineColors | Returns the name, index or rgb strings (hex or , separated) of line color |
GetLineFontIndices | Returns the line font indices: line font to apply to segments in the run (currently 1-7 supported), 0 indicates unknown line font |
GetLineFonts | Returns the names of line font to apply to segments, only used if line_font_index is 0 |
GetLineWidths | Returns the thicknesses of segments (currently 0-2 supported) |
GetRunTypeNames | Returns the names of run type displays |
Enumerations¶
RoutingMechanicalLineColorType Enumeration | Describes the Line color string definition types. |
Method Detail¶
GetIsInitialized¶
-
RoutingMechanical.
GetIsInitialized
¶ Returns the information of whether the mechanical preferences section exists in the application view file.
Signature
GetIsInitialized()
Returns: Return type: bool New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetLineColorTypes¶
-
RoutingMechanical.
GetLineColorTypes
¶ Returns types of string in line_color field.
Valid values are specified by the
NXOpen.Preferences.RoutingMechanicalLineColorType
.Signature
GetLineColorTypes()
Returns: Return type: list of NXOpen.Preferences.RoutingMechanicalLineColorType
New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetLineColors¶
-
RoutingMechanical.
GetLineColors
¶ Returns the name, index or rgb strings (hex or , separated) of line color
Signature
GetLineColors()
Returns: Return type: list of str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetLineFontIndices¶
-
RoutingMechanical.
GetLineFontIndices
¶ Returns the line font indices: line font to apply to segments in the run (currently 1-7 supported), 0 indicates unknown line font
Signature
GetLineFontIndices()
Returns: Return type: list of int New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)
GetLineFonts¶
-
RoutingMechanical.
GetLineFonts
¶ Returns the names of line font to apply to segments, only used if line_font_index is 0
Signature
GetLineFonts()
Returns: Return type: list of str New in version NX4.0.0.
License requirements: routing_advanced (“Routing Advanced”), routing_base (“Routing Basic”)