RoutingMechanicalLineColorType Enumeration

NXOpen.Preferences.RoutingMechanical.LineColorType is an alias for NXOpen.Preferences.RoutingMechanicalLineColorType

class NXOpen.Preferences.RoutingMechanicalLineColorType

Bases: object

Describes the Line color string definition types.

Enum Members

Enum Member Enum Member Description
Unknown
Name
Index
Rgb
Hex
Max
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.