ComponentConstraintDirectionToFixed Enumeration¶
NXOpen.Positioning.ComponentConstraint.DirectionToFixed is an alias for NXOpen.Positioning.ComponentConstraintDirectionToFixed
-
class
NXOpen.Positioning.
ComponentConstraintDirectionToFixed
¶ Bases:
object
Specifies how a constraint affects the positioning of a component.
Enum Members
Enum Member Enum Member Description Unknown No information available Toward Toward fixed geometry AwayFrom Away from fixed geometry NothingFixed The network does not contain any fixed geometry Fix The constraint is a NXOpen.Positioning.ConstraintType.Fix
Suppressed The constraint is suppressed IgnoredInArrangement The current arrangement ignores all constraints -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-