ConstraintType Enumeration¶
NXOpen.Positioning.Constraint.Type is an alias for NXOpen.Positioning.ConstraintType
-
class
NXOpen.Positioning.
ConstraintType
¶ Bases:
object
Specifies the type of a constraint.
Enum Members
Enum Member Enum Member Description Undefined No type Touch Two geometries touch Concentric Two geometries share a center and plane Fix One movable object fixed Distance Two geometries have a specified distance between them Parallel Two geometries are parallel Perpendicular Two geometries are perpendicular Center12 One geometry is positioned mid-way between two others Center22 An implicit plane between two geometries of one movable object is positioned mid-way between two others Angle Two geometries have a specified angle between them Fit Two geometries are coincident Bond A number of movable objects form a rigid group OrientAngle Two geometries have a specified angle between them about an axis SplineData A spline and its defining points SplineLength Constrains the curve length of a spline LinearPattern For internal use only CircularPattern For internal use only Linear2dPattern For internal use only RadiantPattern For internal use only AlignLock Two geometries are constrained to have a common axis and no rotation about it CommonOffsetTransform For internal use only Hinge For internal use only Slider For internal use only Cylindrical For internal use only Ball For internal use only Screw For internal use only Gear For internal use only RackPinion For internal use only Cable For internal use only -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-