PlotColorsWidthsBuilder Class¶
-
class
NXOpen.
PlotColorsWidthsBuilder
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.PlotColorsWidthsBuilder
to be used for plotting.The PlotColorsWidthsBuilder class maintains all colors and widths data, which will be used by the PlotBuilder. If the color option is set to Custom Palette or Colors By Width, the PlotBuilder will translate the CDF object maintained by PlotColorsWidthsBuilder in order to plot with the user-defined colors. If the width option is set to Single Width, Custom Three Width, or Custom Palette, the PlotBuilder will translate the WidthDefinition object maintained by PlotColorsWidthsBuilder in order to plot with the user-defined widths.
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Colors | Returns or sets the color option to be used when plotting. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
UseDrawingSheetColors | Returns or sets the use drawing sheet colors. |
UseDrawingSheetWidths | Returns or sets the use drawing sheet widths. |
Widths | Returns or sets the width option. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
CreateCdf | Creates and returns a NXOpen.CDF object representing the Color Palette. |
CreateWidthDefinition | Creates and returns a NXOpen.WidthDefinition object representing the Width Palette. |
DefinePalette | Initialize the Color Palette. |
DefineWidths | Initialize the Width dialog. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteColors | Delete drawing sheet colors |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DeleteWidths | Delete drawing sheet widths |
EditColors | Edit drawing sheet colors |
EditWidths | Edit drawing sheet widths |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetCdf | Returns a NXOpen.CDF object representing the Color Palette. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
GetWidthDefinition | Returns a NXOpen.WidthDefinition object representing the Width Palette. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
ResetColors | Reset drawing sheet colors |
ResetWidths | Reset drawing sheet widths |
RetrieveColors | Retrieve drawing sheet colors |
RetrieveWidths | Retrieve drawing sheet widths |
SaveColors | Save drawing sheet colors |
SaveWidths | Save drawing sheet widths |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
PlotColorsWidthsBuilderColor Enumeration | Specifies the color option to use when plotting. |
PlotColorsWidthsBuilderWidth Enumeration | Specifies the primary selection of which type of width assignment to use. |
Property Detail¶
Colors¶
-
PlotColorsWidthsBuilder.
Colors
¶ Returns or sets the color option to be used when plotting.
If the color option is set to Custom Palette or Colors By Width then the plotter will use the user defined color attributes belonging to the CDF object.
-------------------------------------
Getter Method
Signature
Colors
Returns: Return type: NXOpen.PlotColorsWidthsBuilderColor
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Colors
Parameters: colors ( NXOpen.PlotColorsWidthsBuilderColor
) –New in version NX5.0.0.
License requirements: None.
IsOccurrence¶
-
PlotColorsWidthsBuilder.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
PlotColorsWidthsBuilder.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
PlotColorsWidthsBuilder.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
PlotColorsWidthsBuilder.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
PlotColorsWidthsBuilder.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
PlotColorsWidthsBuilder.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
UseDrawingSheetColors¶
-
PlotColorsWidthsBuilder.
UseDrawingSheetColors
¶ Returns or sets the use drawing sheet colors.
When this option is set to true, the plotter will use the user-defined drawing sheet colors.
-------------------------------------
Getter Method
Signature
UseDrawingSheetColors
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseDrawingSheetColors
Parameters: useDrawingSheetColors (bool) – New in version NX5.0.0.
License requirements: None.
UseDrawingSheetWidths¶
-
PlotColorsWidthsBuilder.
UseDrawingSheetWidths
¶ Returns or sets the use drawing sheet widths.
When this option is set to true, the plotter will use the user-defined drawing sheet widths.
-------------------------------------
Getter Method
Signature
UseDrawingSheetWidths
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseDrawingSheetWidths
Parameters: useDrawingSheetWidths (bool) – New in version NX5.0.0.
License requirements: None.
Widths¶
-
PlotColorsWidthsBuilder.
Widths
¶ Returns or sets the width option.
If the width option is set to Single Width, Custom Three Widths, or Custom Palette then the plotter will use the user defined width attributes belonging to the WidthDefinition object.
-------------------------------------
Getter Method
Signature
Widths
Returns: Return type: NXOpen.PlotColorsWidthsBuilderWidth
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Widths
Parameters: widths ( NXOpen.PlotColorsWidthsBuilderWidth
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
CreateCdf¶
-
PlotColorsWidthsBuilder.
CreateCdf
¶ Creates and returns a
NXOpen.CDF
object representing the Color Palette.This object contains all custom color information to be used when Custom Palette or Colors By Width is selected from the Color option.
Signature
CreateCdf()
Returns: CDF object Return type: NXOpen.CDF
New in version NX5.0.0.
License requirements: None.
CreateWidthDefinition¶
-
PlotColorsWidthsBuilder.
CreateWidthDefinition
¶ Creates and returns a
NXOpen.WidthDefinition
object representing the Width Palette.This object contains all custom width information to be used when Single Width, Custom Three Widths, or Custom Palette is selected from the Width option.
Signature
CreateWidthDefinition()
Returns: WidthDefinition object Return type: NXOpen.WidthDefinition
New in version NX5.0.0.
License requirements: None.
DefinePalette¶
-
PlotColorsWidthsBuilder.
DefinePalette
¶ Initialize the Color Palette.
This allows the user to change the attributes of any color. These changed colors will be used if Custom Palette or Colors By Width is selected as the color option.
Signature
DefinePalette()
New in version NX5.0.0.
License requirements: None.
DefineWidths¶
-
PlotColorsWidthsBuilder.
DefineWidths
¶ Initialize the Width dialog.
This allows the user to change the attributes of Single Width, Custom Three Widths, or Custom Palette. These changed width values will be used depending on the width option selected.
Signature
DefineWidths()
New in version NX5.0.0.
License requirements: None.
DeleteColors¶
-
PlotColorsWidthsBuilder.
DeleteColors
¶ Delete drawing sheet colors
Signature
DeleteColors()
New in version NX5.0.0.
License requirements: None.
DeleteWidths¶
-
PlotColorsWidthsBuilder.
DeleteWidths
¶ Delete drawing sheet widths
Signature
DeleteWidths()
New in version NX5.0.0.
License requirements: None.
EditColors¶
-
PlotColorsWidthsBuilder.
EditColors
¶ Edit drawing sheet colors
Signature
EditColors()
New in version NX5.0.0.
License requirements: None.
EditWidths¶
-
PlotColorsWidthsBuilder.
EditWidths
¶ Edit drawing sheet widths
Signature
EditWidths()
New in version NX5.0.0.
License requirements: None.
FindObject¶
-
PlotColorsWidthsBuilder.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetCdf¶
-
PlotColorsWidthsBuilder.
GetCdf
¶ Returns a
NXOpen.CDF
object representing the Color Palette.This object contains all custom color information to be used when Custom Palette or Colors By Width is selected from the Color option.
Signature
GetCdf()
Returns: CDF object Return type: NXOpen.CDF
New in version NX5.0.0.
License requirements: None.
GetWidthDefinition¶
-
PlotColorsWidthsBuilder.
GetWidthDefinition
¶ Returns a
NXOpen.WidthDefinition
object representing the Width Palette.This object contains all custom width information to be used when Single Width, Custom Three Widths, or Custom Palette is selected from the Width option.
Signature
GetWidthDefinition()
Returns: WidthDefinition object Return type: NXOpen.WidthDefinition
New in version NX5.0.0.
License requirements: None.
Print¶
-
PlotColorsWidthsBuilder.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
ResetColors¶
-
PlotColorsWidthsBuilder.
ResetColors
¶ Reset drawing sheet colors
Signature
ResetColors()
New in version NX5.0.0.
License requirements: None.
ResetWidths¶
-
PlotColorsWidthsBuilder.
ResetWidths
¶ Reset drawing sheet widths
Signature
ResetWidths()
New in version NX5.0.0.
License requirements: None.
RetrieveColors¶
-
PlotColorsWidthsBuilder.
RetrieveColors
¶ Retrieve drawing sheet colors
Signature
RetrieveColors()
New in version NX5.0.0.
License requirements: None.
RetrieveWidths¶
-
PlotColorsWidthsBuilder.
RetrieveWidths
¶ Retrieve drawing sheet widths
Signature
RetrieveWidths()
New in version NX5.0.0.
License requirements: None.
SaveColors¶
-
PlotColorsWidthsBuilder.
SaveColors
¶ Save drawing sheet colors
Signature
SaveColors()
New in version NX5.0.0.
License requirements: None.
SaveWidths¶
-
PlotColorsWidthsBuilder.
SaveWidths
¶ Save drawing sheet widths
Signature
SaveWidths()
New in version NX5.0.0.
License requirements: None.
SetName¶
-
PlotColorsWidthsBuilder.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.