PartDelayedUpdateStatus Class¶
-
class
NXOpen.
PartDelayedUpdateStatus
¶ Bases:
NXOpen.TransientObject
Represents a list of part names with associated delay status codes.
The status codes serve to communicate delayed update status for the parts that failed to update during Load Interpart Data.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
NumberDelayedParts | Returns the number of parts that could not be updated. |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetDelayedStatus | Returns the delayed update status for a part that failed to update. |
GetPartName | Returns the name of a particular part that could not be updated. |
Structs¶
PartDelayedUpdateStatusDelayStatusInfo_Struct Struct | Logical structure of part delayed update status |
Property Detail¶
Method Detail¶
Dispose¶
-
PartDelayedUpdateStatus.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetDelayedStatus¶
-
PartDelayedUpdateStatus.
GetDelayedStatus
¶ Returns the delayed update status for a part that failed to update.
Signature
GetDelayedStatus(i)
Parameters: i (int) – Index into list of delayed parts Returns: Logical structure of part delayed update status Return type: NXOpen.PartDelayedUpdateStatusDelayStatusInfo_Struct
New in version NX6.0.0.
License requirements: None.