DatabaseObjects Class¶
-
class
NXOpen.PDM.
DatabaseObjects
¶ Bases:
NXOpen.TransientObject
Represents a collection of
NXOpen.PDM.DatabaseObject
.New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Append | This API appends to the collection of NXOpen.PDM.DatabaseObject . |
Dispose | Frees the object from memory. |
GetDatabaseObjects | This API returns the collection of NXOpen.PDM.DatabaseObject as an array. |
SetDatabaseObjects | This API sets the collection of NXOpen.PDM.DatabaseObject . |
Method Detail¶
Append¶
-
DatabaseObjects.
Append
¶ This API appends to the collection of
NXOpen.PDM.DatabaseObject
.Signature
Append(databaseObjects)
Parameters: databaseObjects (list of NXOpen.PDM.DatabaseObjects
) – Database objectsNew in version NX11.0.0.
License requirements: None.
Dispose¶
-
DatabaseObjects.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetDatabaseObjects¶
-
DatabaseObjects.
GetDatabaseObjects
¶ This API returns the collection of
NXOpen.PDM.DatabaseObject
as an array.Signature
GetDatabaseObjects()
Returns: Database objects Return type: list of NXOpen.PDM.DatabaseObject
New in version NX11.0.0.
License requirements: None.
SetDatabaseObjects¶
-
DatabaseObjects.
SetDatabaseObjects
¶ This API sets the collection of
NXOpen.PDM.DatabaseObject
.Signature
SetDatabaseObjects(databaseObjects)
Parameters: databaseObjects (list of NXOpen.PDM.DatabaseObject
) – Database objectsNew in version NX11.0.0.
License requirements: None.