DatabaseObject Class

class NXOpen.PDM.DatabaseObject

Bases: NXOpen.TransientObject

Represents a Teamcenter database object

New in version NX11.0.0.

Methods

Method Description
Dispose Frees the object from memory.

Method Detail

Dispose

DatabaseObject.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX11.0.0.

License requirements: None.