DatabaseObjectManager Class¶
-
class
NXOpen.PDM.
DatabaseObjectManager
¶ Bases:
NXOpen.TransientObject
This class is used for retrieving PDM database objects.
Use
PDM.PdmSession.GetDatabaseObjectManager()
to get the instance of this class.New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
FindObjects | This API finds database objects in the Teamcenter database using a Teamcenter saved query. |
NewDatabaseobjects | This API constructs a new NXOpen.PDM.DatabaseObjects object. |
NewFindcriteria | This API constructs an array of empty NXOpen.PDM.FindCriteria objects. |
Method Detail¶
Dispose¶
-
DatabaseObjectManager.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
FindObjects¶
-
DatabaseObjectManager.
FindObjects
¶ This API finds database objects in the Teamcenter database using a Teamcenter saved query.
Signature
FindObjects(findCriterias)
Parameters: findCriterias (list of NXOpen.PDM.FindCriteria
) – Find critieriaReturns: Database objects Return type: list of NXOpen.PDM.DatabaseObjects
New in version NX11.0.0.
License requirements: None.
NewDatabaseobjects¶
-
DatabaseObjectManager.
NewDatabaseobjects
¶ This API constructs a new
NXOpen.PDM.DatabaseObjects
object.Signature
NewDatabaseobjects()
Returns: Database objects Return type: NXOpen.PDM.DatabaseObjects
New in version NX11.0.0.
License requirements: None.
NewFindcriteria¶
-
DatabaseObjectManager.
NewFindcriteria
¶ This API constructs an array of empty
NXOpen.PDM.FindCriteria
objects.Signature
NewFindcriteria(nCriteria)
Parameters: nCriteria (int) – Returns: Find criteria Return type: list of NXOpen.PDM.FindCriteria
New in version NX11.0.0.
License requirements: None.