OuterEdgesOfFacesRule Class¶
-
class
NXOpen.
OuterEdgesOfFacesRule
¶ Bases:
NXOpen.SelectionIntentRule
Represents a
NXOpen.SelectionIntentRule
that collects the outer edges of a group of faces.New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Type | Returns the get the type of selection intent rule: NXOpen.SelectionIntentRule |
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the Outer Edges of Faces rule: NXOpen.OuterEdgesOfFacesRule |
Method Detail¶
Dispose¶
-
OuterEdgesOfFacesRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX8.5.0.
License requirements: None.
GetData¶
-
OuterEdgesOfFacesRule.
GetData
¶ Gets the data for the Outer Edges of Faces rule:
NXOpen.OuterEdgesOfFacesRule
Signature
GetData()
Returns: Faces or Feature Faces whose boundary edges are used to create this rule Return type: list of NXOpen.NXObject
New in version NX8.5.0.
License requirements: gateway (“UG GATEWAY”)