ImageGroupDocumentData Class¶
-
class
NXOpen.OpenXml.
ImageGroupDocumentData
¶ Bases:
NXOpen.OpenXml.DocumentData
Represents the group of images to be exported to the speific Open XML file.
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
AddImage | Creates a new NXOpen.OpenXml.ImageDocumentData object. |
DeleteAllImages | Deletes all images data |
DeleteNthImage | Deletes the nth image data |
Dispose | Frees the object from memory. |
GetDataType | Gets a specified document data type |
GetImagesCount | Gets the number of images |
GetNthImage | Gets the nth image data |
Method Detail¶
AddImage¶
-
ImageGroupDocumentData.
AddImage
¶ Creates a new
NXOpen.OpenXml.ImageDocumentData
object.Signature
AddImage(fileName, caption)
Parameters: - fileName (str) – the file name of the image data
- caption (str) – the caption of the image data
Returns: the image data
Return type: New in version NX11.0.0.
License requirements: None.
DeleteAllImages¶
-
ImageGroupDocumentData.
DeleteAllImages
¶ Deletes all images data
Signature
DeleteAllImages()
New in version NX11.0.0.
License requirements: None.
DeleteNthImage¶
-
ImageGroupDocumentData.
DeleteNthImage
¶ Deletes the nth image data
Signature
DeleteNthImage(index)
Parameters: index (int) – the index of image New in version NX11.0.0.
License requirements: None.
Dispose¶
-
ImageGroupDocumentData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetImagesCount¶
-
ImageGroupDocumentData.
GetImagesCount
¶ Gets the number of images
Signature
GetImagesCount()
Returns: number of images Return type: int New in version NX11.0.0.
License requirements: None.
GetNthImage¶
-
ImageGroupDocumentData.
GetNthImage
¶ Gets the nth image data
Signature
GetNthImage(index)
Parameters: index (int) – the index of image data Returns: the image data Return type: NXOpen.OpenXml.ImageDocumentData
New in version NX11.0.0.
License requirements: None.