ImageDocumentData Class¶
-
class
NXOpen.OpenXml.
ImageDocumentData
¶ Bases:
NXOpen.OpenXml.DocumentData
Represents the image to be exported to the speific Open XML file.
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetCaption | Gets the caption of the image data |
GetDataType | Gets a specified document data type |
GetFileName | Gets the file name of the image data |
SetCaption | Sets the caption of the image data |
SetFileName | Sets the file name of the image data |
Enumerations¶
ImageDocumentDataCaptionPosition Enumeration | the location of the caption for image data |
Method Detail¶
Dispose¶
-
ImageDocumentData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.