ImageDocumentDataCaptionPosition Enumeration
NXOpen.OpenXml.ImageDocumentData.CaptionPosition is an alias for NXOpen.OpenXml.ImageDocumentDataCaptionPosition
-
class
NXOpen.OpenXml.
ImageDocumentDataCaptionPosition
Bases: object
the location of the caption for image data
Enum Members
Enum Member |
Enum Member Description |
Above |
the above position |
Bellow |
the bellow position |
-
ValueOf
()
Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature ValueOf(value)
Parameters: | value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. |
Return type: | Enum Member type. |
License requirements: None.