TirePropertyBasicCollection Class¶
-
class
NXOpen.Motion.
TirePropertyBasicCollection
¶ Bases:
object
Represents a collection of
NXOpen.Motion.TirePropertyBasic
elementsTo obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateTirePropertyBasicBuilder | Return NXOpen.Motion.TirePropertyBasicBuilder object |
FindObject | Finds the NXOpen.Motion.TirePropertyBasic with the given name. |
Method Detail¶
CreateTirePropertyBasicBuilder¶
-
TirePropertyBasicCollection.
CreateTirePropertyBasicBuilder
¶ Return
NXOpen.Motion.TirePropertyBasicBuilder
objectSignature
CreateTirePropertyBasicBuilder(tireProperty)
Parameters: tireProperty ( NXOpen.Motion.TirePropertyBasic
) –NXOpen.Motion.TirePropertyBasic
to be edited, if None then create a new oneReturns: TirePropertyBasicBuilder object Return type: NXOpen.Motion.TirePropertyBasicBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
TirePropertyBasicCollection.
FindObject
¶ Finds the
NXOpen.Motion.TirePropertyBasic
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.TirePropertyBasic
Returns: NXOpen.Motion.TirePropertyBasic
with this nameReturn type: NXOpen.Motion.TirePropertyBasic
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)