TirePropertyBasicBuilder Class¶
-
class
NXOpen.Motion.
TirePropertyBasicBuilder
¶ Bases:
NXOpen.Motion.TirePropertyBuilder
Represents a builder for a
Motion.TirePropertyBasic
To create a new instance of this class, use
NXOpen.Motion.TirePropertyBasicCollection.CreateTirePropertyBasicBuilder()
Default values.
Property Value AdvancedTab.AligningMomentArm.Value 0.0 (millimeters part), 0.0 (inches part) AdvancedTab.ConeIndex.Value 0.0 (millimeters part), 0.0 (inches part) AdvancedTab.ContactAreaType Function AdvancedTab.DistributedContact 0 AdvancedTab.FrictionType Function AdvancedTab.NumDivisions.Value 1 (millimeters part), 1 (inches part) AdvancedTab.RelaxationLength.Value 0.0 (millimeters part), 0.0 (inches part) AdvancedTab.RollingRadiusType None AdvancedTab.RollingRadiusValue.Value 0.0 (millimeters part), 0.0 (inches part) AdvancedTab.SectionHeight.Value 0.0 (millimeters part), 0.0 (inches part) AdvancedTab.SectionWidth.Value 0.0 (millimeters part), 0.0 (inches part) AdvancedTab.StaticHold 1 AdvancedTab.SurfaceType Simple AdvancedTab.TransDampingDeflection.Value 0.0 (millimeters part), 0.0 (inches part) BasicTab.CorneringStiffness.Value 1000000.0 (millimeters part), 224808.944 (inches part) BasicTab.FrictionCoefficient.Value 1.0 (millimeters part), 1.0 (inches part) BasicTab.LateralForceType Cornering BasicTab.Radius.Value 300 (millimeters part), 11.811 (inches part) BasicTab.RollingResistance.Value 0.0 (millimeters part), 0.0 (inches part) BasicTab.VerticalDamping.DataType Expression HighOrderEffectsTab.CarcassMass.Value 0.0 (millimeters part), 0.0 (inches part) HighOrderEffectsTab.LateralDamping.Value 0 (millimeters part), 0 (inches part) HighOrderEffectsTab.LateralStiffness.Value 0 (millimeters part), 0 (inches part) HighOrderEffectsTab.LongDamping.Value 0 (millimeters part), 0 (inches part) HighOrderEffectsTab.LongStiffness.Value 0 (millimeters part), 0 (inches part) HighOrderEffectsTab.RollMoment 1 HighOrderEffectsTab.UnloadingVerticalStiffnessType Function HighOrderEffectsTab.VerticalStiffnessTransVelocity.Value 10 (millimeters part), 0.393701 (inches part) New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AdvancedTab | Returns the advancedTab. |
BasicTab | Returns the basicTab. |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
HighOrderEffectsTab | Returns the highOrderTab. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AdvancedTab¶
-
TirePropertyBasicBuilder.
AdvancedTab
¶ Returns the advancedTab.
This is a builder for the parameters in the TirePropertyBasic UI Advanced tab.
-------------------------------------
Getter Method
Signature
AdvancedTab
Returns: Return type: NXOpen.Motion.TirePropertyAdvancedParameters
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
BasicTab¶
-
TirePropertyBasicBuilder.
BasicTab
¶ Returns the basicTab.
This is a builder for the parameters in the TirePropertyBasic UI Basic tab.
-------------------------------------
Getter Method
Signature
BasicTab
Returns: Return type: NXOpen.Motion.TirePropertyBasicParameters
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
HighOrderEffectsTab¶
-
TirePropertyBasicBuilder.
HighOrderEffectsTab
¶ Returns the highOrderTab.
This is a builder for the parameters in the TirePropertyBasic UI High Order Effects tab.
-------------------------------------
Getter Method
Signature
HighOrderEffectsTab
Returns: Return type: NXOpen.Motion.TirePropertyHighOrderParameters
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
TirePropertyBasicBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.