PlantInputCollection Class¶
-
class
NXOpen.Motion.
PlantInputCollection
¶ Bases:
object
Represents a collection of Plant Input objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreatePlantInputBuilder | Creates a NXOpen.Motion.PlantInputBuilder |
FindObject | Finds the NXOpen.Motion.PlantInput with the given name. |
Method Detail¶
CreatePlantInputBuilder¶
-
PlantInputCollection.
CreatePlantInputBuilder
¶ Creates a
NXOpen.Motion.PlantInputBuilder
Signature
CreatePlantInputBuilder(plantinput)
Parameters: plantinput ( NXOpen.Motion.PlantInput
) –Returns: Return type: NXOpen.Motion.PlantInputBuilder
New in version NX6.0.0.
License requirements: nx_motion_cosim (“NX Motion CoSimulation”)
FindObject¶
-
PlantInputCollection.
FindObject
¶ Finds the
NXOpen.Motion.PlantInput
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.PlantInput
.Returns: NXOpen.Motion.PlantInput
with this name.Return type: NXOpen.Motion.PlantInput
New in version NX6.0.0.
License requirements: nx_motion_cosim (“NX Motion CoSimulation”)