PhysicsConversionBuilder Class¶
-
class
NXOpen.Motion.
PhysicsConversionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Motion.PhysicsConversionBuilder
builderTo create a new instance of this class, use
NXOpen.Motion.MotionSession.CreatePhysicsConversionBuilder()
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
ActiveAll | The active button. |
Commit | Commits any edits that have been applied to the builder. |
DeactiveAll | The deactive button. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetPhysics | The physics data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateStatus | The data update accordingly. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
ActiveAll¶
-
PhysicsConversionBuilder.
ActiveAll
¶ The active button.
Call this method to make all physics items active.
Signature
ActiveAll()
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
DeactiveAll¶
-
PhysicsConversionBuilder.
DeactiveAll
¶ The deactive button.
Call this method to make all physics items inactive.
Signature
DeactiveAll()
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetPhysics¶
-
PhysicsConversionBuilder.
GetPhysics
¶ The physics data.
Call this method to get the physics data.
Signature
GetPhysics()
Returns: a tuple Return type: A tuple consisting of (physicsProto, partOccurrence). physicsProto is a list of NXOpen.NXObject
. partOccurrence is a list ofNXOpen.Assemblies.Component
.New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
UpdateStatus¶
-
PhysicsConversionBuilder.
UpdateStatus
¶ The data update accordingly.
Call this method to make part of the physics items active or inactive.
Signature
UpdateStatus(physicsProto, partOccurrence, active)
Parameters: - physicsProto (list of
NXOpen.NXObject
) – - partOccurrence (list of
NXOpen.Assemblies.Component
) – - active (bool) –
New in version NX8.0.0.
License requirements: mechanisms (“MECHANISMS”)
- physicsProto (list of
Validate¶
-
PhysicsConversionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.