MotionMethods Class¶
-
class
NXOpen.Motion.
MotionMethods
¶ Bases:
object
Represents a
NXOpen.Motion.MotionMethods
classTo obtain an instance of this class, refer to
NXOpen.Motion.MotionSession
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CopyConnectorParameters | Copies the connector parameters |
CopyParameters | Copy parameters from source to destination. |
ExportParameters | Export parameters of an entity into a txt file. |
ImportParameters | Import parameters of an object into a txt file. |
ModelCheck | Check all motion objects |
Method Detail¶
CopyConnectorParameters¶
-
MotionMethods.
CopyConnectorParameters
¶ Copies the connector parameters
Signature
CopyConnectorParameters(sourceConnector, destinationConnector)
Parameters: - sourceConnector (
NXOpen.NXObject
) – Source connector from which parameters are copied - destinationConnector (
NXOpen.NXObject
) – Destination connector to which the parameters are copied
New in version NX8.0.0.
Deprecated since version NX12.0.0: Use
MotionMethods.CopyParameters()
instead.License requirements: mechanisms (“MECHANISMS”)
- sourceConnector (
CopyParameters¶
-
MotionMethods.
CopyParameters
¶ Copy parameters from source to destination.
Source and Destination must be of the same type. Only objects that support this command in Motion Navigator are supported.
Signature
CopyParameters(source, destination)
Parameters: - source (
NXOpen.NXObject
) – Source object from which parameters are copied - destination (
NXOpen.NXObject
) – Destination object to which the parameters are copied
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
- source (
ExportParameters¶
-
MotionMethods.
ExportParameters
¶ Export parameters of an entity into a txt file.
Only objects that support this command in Motion Navigator are supported.
Signature
ExportParameters(entity, fileName)
Parameters: - entity (
NXOpen.NXObject
) – entity to export - fileName (str) – file to export to
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
- entity (
ImportParameters¶
-
MotionMethods.
ImportParameters
¶ Import parameters of an object into a txt file.
Only objects that support this command in Motion Navigator are supported.
Signature
ImportParameters(entity, fileName)
Parameters: - entity (
NXOpen.NXObject
) – entity to import - fileName (str) – file to import from
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
- entity (