LinkDriverCollection Class¶
-
class
NXOpen.Motion.
LinkDriverCollection
¶ Bases:
object
Represents a collection of LinkDriver objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateLinkDriverBuilder | Creates a NXOpen.Motion.LinkDriverBuilder |
FindObject | Finds the NXOpen.Motion.LinkDriver object with the given name. |
Method Detail¶
CreateLinkDriverBuilder¶
-
LinkDriverCollection.
CreateLinkDriverBuilder
¶ Creates a
NXOpen.Motion.LinkDriverBuilder
Signature
CreateLinkDriverBuilder(linkDriver)
Parameters: linkDriver ( NXOpen.Motion.LinkDriver
) –NXOpen.Motion.LinkDriver
to be editedReturns: LinkDriverBuilder object Return type: NXOpen.Motion.LinkDriverBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
LinkDriverCollection.
FindObject
¶ Finds the
NXOpen.Motion.LinkDriver
object with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.LinkDriver
.Returns: NXOpen.Motion.LinkDriver
with this name.Return type: NXOpen.Motion.LinkDriver
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)