LinkDriverBuilder Class¶
-
class
NXOpen.Motion.
LinkDriverBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.LinkDriverBuilder
To create a new instance of this class, use
NXOpen.Motion.LinkDriverCollection.CreateLinkDriverBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ActionLinkAttachment | Returns the Action Link Attachment |
BaseLinkAttachment | Returns the Base Link Attachment |
DisplayScale | Returns or sets the icon display scale |
DriverMotions | Returns the Driver Motions |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Name | Returns or sets the name |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ActionLinkAttachment¶
-
LinkDriverBuilder.
ActionLinkAttachment
¶ Returns the Action Link Attachment
-------------------------------------
Getter Method
Signature
ActionLinkAttachment
Returns: Return type: NXOpen.Motion.LinkAttachmentData
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
BaseLinkAttachment¶
-
LinkDriverBuilder.
BaseLinkAttachment
¶ Returns the Base Link Attachment
-------------------------------------
Getter Method
Signature
BaseLinkAttachment
Returns: Return type: NXOpen.Motion.LinkAttachmentData
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
DriverMotions¶
-
LinkDriverBuilder.
DriverMotions
¶ Returns the Driver Motions
-------------------------------------
Getter Method
Signature
DriverMotions
Returns: Return type: NXOpen.Motion.DriverMotionsData
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Name¶
-
LinkDriverBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
LinkDriverBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.