CouplerCableBuilder Class¶
-
class
NXOpen.Motion.
CouplerCableBuilder
¶ Bases:
NXOpen.Motion.CouplerBuilder
Represents a
NXOpen.Motion.CouplerCableBuilder
To create a new instance of this class, use
NXOpen.Motion.CouplerCollection.CreateCouplerCableBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ContactPoint | Returns or sets the contact point |
DisplayScale | Returns or sets the icon display scale |
FirstJoint | Returns the first joint |
FirstRadiusExpression | Returns the first radius expression. |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Name | Returns or sets the name |
RatioExpression | Returns the ratio expression |
SecondJoint | Returns the second joint |
SecondRadiusExpression | Returns the second radius expression. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
Validate¶
-
CouplerCableBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.