CouplerBuilder Class¶
-
class
NXOpen.Motion.
CouplerBuilder
¶ Bases:
NXOpen.Motion.MotionBuilder
Represents a
NXOpen.Motion.CouplerBuilder
This is an abstract class, and cannot be created.
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ContactPoint | Returns or sets the contact point |
DisplayScale | Returns or sets the icon display scale |
FirstJoint | Returns the first joint |
FirstRadiusExpression | Returns the first radius expression. |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
Name | Returns or sets the name |
RatioExpression | Returns the ratio expression |
SecondJoint | Returns the second joint |
SecondRadiusExpression | Returns the second radius expression. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ContactPoint¶
-
CouplerBuilder.
ContactPoint
¶ Returns or sets the contact point
-------------------------------------
Getter Method
Signature
ContactPoint
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContactPoint
Parameters: contactPt ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
FirstJoint¶
-
CouplerBuilder.
FirstJoint
¶ Returns the first joint
-------------------------------------
Getter Method
Signature
FirstJoint
Returns: Return type: NXOpen.Motion.SelectJoint
New in version NX6.0.0.
License requirements: None.
FirstRadiusExpression¶
-
CouplerBuilder.
FirstRadiusExpression
¶ Returns the first radius expression.
Only valid when using Simcenter Solver.
-------------------------------------
Getter Method
Signature
FirstRadiusExpression
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
Name¶
-
CouplerBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX6.0.0.
License requirements: None.
RatioExpression¶
-
CouplerBuilder.
RatioExpression
¶ Returns the ratio expression
-------------------------------------
Getter Method
Signature
RatioExpression
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
SecondJoint¶
-
CouplerBuilder.
SecondJoint
¶ Returns the second joint
-------------------------------------
Getter Method
Signature
SecondJoint
Returns: Return type: NXOpen.Motion.SelectJoint
New in version NX6.0.0.
License requirements: None.
SecondRadiusExpression¶
-
CouplerBuilder.
SecondRadiusExpression
¶ Returns the second radius expression.
Only valid when using Simcenter Solver.
-------------------------------------
Getter Method
Signature
SecondRadiusExpression
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CouplerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.