BodyContactLms Class¶
-
class
NXOpen.Motion.
BodyContactLms
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.Motion.BodyContactLms
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ActionAngleTolerance | Returns the action angle tolerance |
ActionDistanceTolerance | Returns the action distance tolerance |
ActionEnableMaxFacetSize | Returns or sets the action enable max facet size |
ActionMaxFacetSize | Returns the action max facet size |
ActionTessellationFile | Returns or sets the action tessellation file |
ActionUseTessellationFile | Returns or sets the action tessellation file option |
BaseAngleTolerance | Returns the base angle tolerance |
BaseDistanceTolerance | Returns the base distance tolerance |
BaseEnableMaxFacetSize | Returns or sets the base enable max facet size |
BaseMaxFacetSize | Returns the base max facet size |
BaseTessellationFile | Returns or sets the base tessellation file |
BaseUseTessellationFile | Returns or sets the base tessellation file option |
CoulombFrictionOption | Returns or sets the coulomb friction option |
DynamicCoefficient | Returns the dynamic coefficient |
ForceExponent | Returns the force exponent |
ForceModel | Returns or sets the force model |
ForceModelTolerance | Returns the force model tolerance |
FrictionVelocity | Returns the friction velocity |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MaterialDamping | Returns the material damping |
MaxPenetrationDepth | Returns the max penetration depth |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
StaticCoefficient | Returns the static coefficient |
StictionVelocity | Returns the stiction velocity |
Stiffness | Returns the stiffness |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Enumerations¶
BodyContactLmsCoulombFriction Enumeration | the enum for friction option of 3D contact |
BodyContactLmsForceModelType Enumeration | the enum for force model of 3D contact |
Property Detail¶
ActionAngleTolerance¶
-
BodyContactLms.
ActionAngleTolerance
¶ Returns the action angle tolerance
-------------------------------------
Getter Method
Signature
ActionAngleTolerance
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ActionDistanceTolerance¶
-
BodyContactLms.
ActionDistanceTolerance
¶ Returns the action distance tolerance
-------------------------------------
Getter Method
Signature
ActionDistanceTolerance
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ActionEnableMaxFacetSize¶
-
BodyContactLms.
ActionEnableMaxFacetSize
¶ Returns or sets the action enable max facet size
-------------------------------------
Getter Method
Signature
ActionEnableMaxFacetSize
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActionEnableMaxFacetSize
Parameters: actionEnableMaxFacetSize (bool) – New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
ActionMaxFacetSize¶
-
BodyContactLms.
ActionMaxFacetSize
¶ Returns the action max facet size
-------------------------------------
Getter Method
Signature
ActionMaxFacetSize
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ActionTessellationFile¶
-
BodyContactLms.
ActionTessellationFile
¶ Returns or sets the action tessellation file
-------------------------------------
Getter Method
Signature
ActionTessellationFile
Returns: Return type: str New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ActionTessellationFile
Parameters: fileName (str) – New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
ActionUseTessellationFile¶
-
BodyContactLms.
ActionUseTessellationFile
¶ Returns or sets the action tessellation file option
-------------------------------------
Getter Method
Signature
ActionUseTessellationFile
Returns: Return type: bool New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ActionUseTessellationFile
Parameters: fileOption (bool) – New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
BaseAngleTolerance¶
-
BodyContactLms.
BaseAngleTolerance
¶ Returns the base angle tolerance
-------------------------------------
Getter Method
Signature
BaseAngleTolerance
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
BaseDistanceTolerance¶
-
BodyContactLms.
BaseDistanceTolerance
¶ Returns the base distance tolerance
-------------------------------------
Getter Method
Signature
BaseDistanceTolerance
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
BaseEnableMaxFacetSize¶
-
BodyContactLms.
BaseEnableMaxFacetSize
¶ Returns or sets the base enable max facet size
-------------------------------------
Getter Method
Signature
BaseEnableMaxFacetSize
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BaseEnableMaxFacetSize
Parameters: baseEnableMaxFacetSize (bool) – New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
BaseMaxFacetSize¶
-
BodyContactLms.
BaseMaxFacetSize
¶ Returns the base max facet size
-------------------------------------
Getter Method
Signature
BaseMaxFacetSize
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
BaseTessellationFile¶
-
BodyContactLms.
BaseTessellationFile
¶ Returns or sets the base tessellation file
-------------------------------------
Getter Method
Signature
BaseTessellationFile
Returns: Return type: str New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
BaseTessellationFile
Parameters: fileName (str) – New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
BaseUseTessellationFile¶
-
BodyContactLms.
BaseUseTessellationFile
¶ Returns or sets the base tessellation file option
-------------------------------------
Getter Method
Signature
BaseUseTessellationFile
Returns: Return type: bool New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
BaseUseTessellationFile
Parameters: fileOption (bool) – New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
CoulombFrictionOption¶
-
BodyContactLms.
CoulombFrictionOption
¶ Returns or sets the coulomb friction option
-------------------------------------
Getter Method
Signature
CoulombFrictionOption
Returns: Return type: NXOpen.Motion.BodyContactLmsCoulombFriction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CoulombFrictionOption
Parameters: coulombFrictionOption ( NXOpen.Motion.BodyContactLmsCoulombFriction
) –New in version NX10.0.0.
License requirements: mechanisms (“MECHANISMS”)
DynamicCoefficient¶
-
BodyContactLms.
DynamicCoefficient
¶ Returns the dynamic coefficient
-------------------------------------
Getter Method
Signature
DynamicCoefficient
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ForceExponent¶
-
BodyContactLms.
ForceExponent
¶ Returns the force exponent
-------------------------------------
Getter Method
Signature
ForceExponent
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
ForceModel¶
-
BodyContactLms.
ForceModel
¶ Returns or sets the force model
-------------------------------------
Getter Method
Signature
ForceModel
Returns: Return type: NXOpen.Motion.BodyContactLmsForceModelType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForceModel
Parameters: model ( NXOpen.Motion.BodyContactLmsForceModelType
) –New in version NX11.0.0.
License requirements: None.
ForceModelTolerance¶
-
BodyContactLms.
ForceModelTolerance
¶ Returns the force model tolerance
-------------------------------------
Getter Method
Signature
ForceModelTolerance
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
FrictionVelocity¶
-
BodyContactLms.
FrictionVelocity
¶ Returns the friction velocity
-------------------------------------
Getter Method
Signature
FrictionVelocity
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
IsOccurrence¶
-
BodyContactLms.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
BodyContactLms.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
MaterialDamping¶
-
BodyContactLms.
MaterialDamping
¶ Returns the material damping
-------------------------------------
Getter Method
Signature
MaterialDamping
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
MaxPenetrationDepth¶
-
BodyContactLms.
MaxPenetrationDepth
¶ Returns the max penetration depth
-------------------------------------
Getter Method
Signature
MaxPenetrationDepth
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Name¶
-
BodyContactLms.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
BodyContactLms.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
BodyContactLms.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
BodyContactLms.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
StaticCoefficient¶
-
BodyContactLms.
StaticCoefficient
¶ Returns the static coefficient
-------------------------------------
Getter Method
Signature
StaticCoefficient
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
StictionVelocity¶
-
BodyContactLms.
StictionVelocity
¶ Returns the stiction velocity
-------------------------------------
Getter Method
Signature
StictionVelocity
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Stiffness¶
-
BodyContactLms.
Stiffness
¶ Returns the stiffness
-------------------------------------
Getter Method
Signature
Stiffness
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
FindObject¶
-
BodyContactLms.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
BodyContactLms.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
BodyContactLms.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.