ArticulationControl Class¶
-
class
NXOpen.Motion.
ArticulationControl
¶ Bases:
NXOpen.Motion.PostControl
Represents the
NXOpen.Motion.ArticulationControl
An instance of this class can not be obtained
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActiveView | Returns or sets the active view |
Delay | Returns or sets the articulation delay |
IsOccurrence | Returns whether this object is an occurrence or not. |
JointsLimits | Returns or sets the articulation joint limits setting |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ArticulationSolve | Articulation solve with joint driver step size and number of step as input This method adds event loop that solves step by step and return. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Finish | Articulation finish |
GetArticulationJoints | Articulation joints |
GetArticulationJointsDisplacement | Get the articulation joints displacement |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
StepToAssemblyPosition | Articulation to assembly position |
StepToDesignPosition | Articulation to design position |
Stop | Articulation stop |
Property Detail¶
ActiveView¶
-
ArticulationControl.
ActiveView
¶ Returns or sets the active view
-------------------------------------
Getter Method
Signature
ActiveView
Returns: The articulation active view Return type: NXOpen.Motion.ActiveView
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ActiveView
Parameters: activeView ( NXOpen.Motion.ActiveView
) –New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
Delay¶
-
ArticulationControl.
Delay
¶ Returns or sets the articulation delay
-------------------------------------
Getter Method
Signature
Delay
Returns: The articulation delay Return type: int New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Delay
Parameters: delay (int) – New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
IsOccurrence¶
-
ArticulationControl.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JointsLimits¶
-
ArticulationControl.
JointsLimits
¶ Returns or sets the articulation joint limits setting
-------------------------------------
Getter Method
Signature
JointsLimits
Returns: The joint limits on/off flag setting Return type: bool New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
JointsLimits
Parameters: jointLimits (bool) – New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
JournalIdentifier¶
-
ArticulationControl.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ArticulationControl.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ArticulationControl.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ArticulationControl.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ArticulationControl.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
ArticulationSolve¶
-
ArticulationControl.
ArticulationSolve
¶ Overloaded method ArticulationSolve
ArticulationSolve(numSteps, jointTags, stepSize, stepSizeUnit)
ArticulationSolve(jointTags, displacement, displacementUnit)
-------------------------------------
Articulation solve with joint driver step size and number of step as input This method adds event loop that solves step by step and return. It does not wait finishing the solving process. For the case there is no UI button to control the solve and stop action, call another
Motion.ArticulationControl.ArticulationSolve()
that has no numSteps input in a cycle to solveSignature
ArticulationSolve(numSteps, jointTags, stepSize, stepSizeUnit)
Parameters: - numSteps (int) – The number of step will take in one action
- jointTags (list of
NXOpen.Motion.Joint
) – Articulation joint tags - stepSize (list of float) – Articulation joint step size
- stepSizeUnit (list of
NXOpen.Unit
) – Articulation joint step size unit
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Articulation solve with joint driver displacement as input
Signature
ArticulationSolve(jointTags, displacement, displacementUnit)
Parameters: - jointTags (list of
NXOpen.Motion.Joint
) – Articulation joint tags - displacement (list of float) – Articulation joint displacement
- displacementUnit (list of
NXOpen.Unit
) – Articulation joint displacement units
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
FindObject¶
-
ArticulationControl.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Finish¶
-
ArticulationControl.
Finish
¶ Articulation finish
Signature
Finish()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetArticulationJoints¶
-
ArticulationControl.
GetArticulationJoints
¶ Articulation joints
Signature
GetArticulationJoints()
Returns: The articulation joint array Return type: list of NXOpen.Motion.Joint
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
GetArticulationJointsDisplacement¶
-
ArticulationControl.
GetArticulationJointsDisplacement
¶ Get the articulation joints displacement
Signature
GetArticulationJointsDisplacement(jointTag)
Parameters: jointTag ( NXOpen.Motion.Joint
) – The special articulation joint objectReturns: a tuple Return type: A tuple consisting of (currentStep, displacement, displacementUnit). currentStep is a int. The current step index displacement is a float. The articulation joint displacement value within current step displacementUnit is a NXOpen.Unit
. The articulation joint displacement unitNew in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
Print¶
-
ArticulationControl.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
ArticulationControl.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
StepToAssemblyPosition¶
-
ArticulationControl.
StepToAssemblyPosition
¶ Articulation to assembly position
Signature
StepToAssemblyPosition()
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)