ModelingView Class¶
-
class
NXOpen.
ModelingView
¶ Bases:
NXOpen.View
Represents a Modeling View
Modeling Views may only be created by Save As.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AbsoluteOrigin | Returns the view origin in absolute space. |
ActiveDynamicSection | Returns or sets the active dynamic section object in the modeling view. |
DisclosurePurpose | Returns or sets the Disclosure Purpose. |
DisplaySectioningToggle | Returns or sets the toggle between enabling or disabling the Dynamic Sectioning viewing |
IsMirrored | Returns a flag indicating whether the model view is mirrored |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LockRotations | Returns or sets the Lock Rotations toggle state of a view. |
Matrix | Returns the view matrix. |
Name | Returns the custom name of the object. |
Origin | Returns the view origin. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
RenderingStyle | Returns or sets the rendering style of the view. |
Scale | Returns the view scale. |
SyncViews | Returns or sets the Synchronized Views toggle state of a view. |
Tag | Returns the Tag for this object. |
TriadVisibility | Returns or sets the visibility of the view triad in the view. |
WcsVisibility | Returns or sets the visibility of the WCS in the view. |
HiqhQualityImage | Returns the High Quality Image instance belonging to a view |
Methods¶
Method | Description |
---|---|
AskVisibleObjects | Returns an array of objects visible in a view. |
ChangePerspective | Changes a view from an orthographic view to a perspective view, or from a perspective view to an orthographic view. |
Concatenate | Concatenates the given translation with the previous viewing transformation of the specified view. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
Expand | Expands the specified view to fill as much of the layout which contains the view as possible, without changing the aspect ratio of the view. |
ExpandCollapseNode | Expand or collapse the node for the specified Model View in the Part Navigator. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
Fit | Adjusts the bounds of a given view so that it fully encompasses the extents of the model geometry. |
FitAfterShowOrHide | Adjusts the bounds of a given view conditionally so that it fully encompasses the extents of the model geometry. |
FitToObjects | Adjusts the bounds of a given view so that it fully encompasses the extents of the given objects. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetAxis | Returns one of the view axes. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetExpandedScale | Returns the view scale, including any expansion factor. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasPreview | Returns whether or not the given view has a preview. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
IsDynamicSectionVisible | Returns if the specified dynamic section object is visible in this view. |
MakeWork | Makes the given view the work view. |
Orient | Changes the view orientation relative to the specified absolute coordinate system. |
Prints a representation of this object to the system log file. | |
Regenerate | Regenerates the display of given view. |
Restore | Restores a view to its last remembered rotation, scale and translation. |
Rotate | Rotates the view by concatenating the given matrix to the existing rotation matrix of the view. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDynamicSectionVisible | Sets the specified dynamic section object is visible/invisible in this view. |
SetName | Sets the custom name of the object. |
SetOrigin | Moves the given position to the center of the view. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetRotationTranslationScale | Sets the rotation, translation and scale of the specified view. |
SetScale | Sets the scale of the specified view to the desired scale factor. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
SnapToClosestCannedOrientation | Changes the orientation of the given view to the orientation of the canned view whose orientation is the closest to that of the given view. |
SnapToVariantCannedOrientation | Similar to NXOpen.View.SnapToClosestCannedOrientation() except it changes the orientation of the given view to the orientation of some canned view variant based on I-deas’s ‘snapview’ logic whose orientation is the closest to one of the six orthographic and eight flavors of trimetric views. |
UpdateCustomSymbols | Updates custom symbol in a drawing member view or drawing sheet |
UpdateDisplay | Updates the display of given view, as needed. |
UseDefaultLights | Changes the set of lights used in the given view to the Default set, which for now is the Scene Ambient, Scene Left Top and Scene Right Top lights. |
UseSceneLights | Changes the set of lights used in the given view to the Scene set, which for now includes the eight predefined scene lights (including the Scene Ambient light). |
Zoom | Scales the specified view to a desired relative scale. |
ZoomAboutPoint | Scales the specified view such that the given scale_about_point does not move. |
ZoomByRectangle | Scales the specified view such that the specified rectangle is as large as possible while being fully contained within the viewport. |
Property Detail¶
ActiveDynamicSection¶
-
ModelingView.
ActiveDynamicSection
¶ Returns or sets the active dynamic section object in the modeling view.
Each modeling view can contain one and only one active dynamic section. Trying to reset the active dynamic section in the view by specifying None dynamic section will raise an error.
-------------------------------------
Getter Method
Signature
ActiveDynamicSection
Returns: active dynamic section Return type: NXOpen.Display.DynamicSection
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActiveDynamicSection
Parameters: dynamicSection ( NXOpen.Display.DynamicSection
) – Dynamic section object. Specify None to reset active dynamic section.New in version NX6.0.0.
License requirements: None.
DisplaySectioningToggle¶
-
ModelingView.
DisplaySectioningToggle
¶ Returns or sets the toggle between enabling or disabling the Dynamic Sectioning viewing
-------------------------------------
Getter Method
Signature
DisplaySectioningToggle
Returns: See if dyanamic Sectioning display is enabled Return type: bool New in version NX4.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplaySectioningToggle
Parameters: newState (bool) – To enable or disable dyanamic Sectioning on display New in version NX4.0.0.
License requirements: None.
IsMirrored¶
-
ModelingView.
IsMirrored
¶ Returns a flag indicating whether the model view is mirrored
-------------------------------------
Getter Method
Signature
IsMirrored
Returns: Mirrored flag Return type: bool New in version NX8.5.0.
License requirements: None.
IsOccurrence¶
-
ModelingView.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ModelingView.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
ModelingView.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
ModelingView.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ModelingView.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
ModelingView.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
HiqhQualityImage¶
-
ModelingView.
HiqhQualityImage
¶ Returns the High Quality Image instance belonging to a view
Signature
HiqhQualityImage
New in version NX3.0.0.
Returns: Return type: NXOpen.ModelingViewHighQualityImage
Method Detail¶
ExpandCollapseNode¶
-
ModelingView.
ExpandCollapseNode
¶ Expand or collapse the node for the specified Model View in the Part Navigator.
Signature
ExpandCollapseNode(expand)
Parameters: expand (bool) – New in version NX9.0.3.
License requirements: None.
FindObject¶
-
ModelingView.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
IsDynamicSectionVisible¶
-
ModelingView.
IsDynamicSectionVisible
¶ Returns if the specified dynamic section object is visible in this view.
When dynamic section object is visible, the section curves are shown in the view.
Signature
IsDynamicSectionVisible(dynamicSection)
Parameters: dynamicSection ( NXOpen.Display.DynamicSection
) – Dynamic section objectReturns: Visibility flag Return type: bool New in version NX6.0.0.
License requirements: None.
Print¶
-
ModelingView.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetDynamicSectionVisible¶
-
ModelingView.
SetDynamicSectionVisible
¶ Sets the specified dynamic section object is visible/invisible in this view.
When dynamic section object is visible, the section curves are shown in the view. Showing section objects in a view is a performance intensive operation. In involves cutting all visible bodies in the view with the section object definition.
Signature
SetDynamicSectionVisible(dynamicSection, visible)
Parameters: - dynamicSection (
NXOpen.Display.DynamicSection
) – Dynamic section object - visible (bool) – Visibility flag
New in version NX6.0.0.
License requirements: None.
- dynamicSection (
SetName¶
-
ModelingView.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
UseDefaultLights¶
-
ModelingView.
UseDefaultLights
¶ Changes the set of lights used in the given view to the “Default” set, which for now is the Scene Ambient, Scene Left Top and Scene Right Top lights.
If the definition of the “Default” set should ever change, the implementation of this method would change accordingly.
Signature
UseDefaultLights()
New in version NX4.0.0.
License requirements: None.
UseSceneLights¶
-
ModelingView.
UseSceneLights
¶ Changes the set of lights used in the given view to the “Scene” set, which for now includes the eight predefined scene lights (including the Scene Ambient light).
If the definition of the “Scene” set should ever change, the implementation of this method would change accordingly.
Signature
UseSceneLights()
New in version NX4.0.0.
License requirements: None.