Blank |
Blanks the object. |
CreateAttributeIterator |
Create an attribute iterator |
DeleteAllAttributesByType |
Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle |
Deletes an attribute by type and title. |
DeleteUserAttribute |
Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes |
Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject |
Finds the Mfg.Mlp.MachiningFeature with the given identifier as recorded in a journal. |
GetAttributeTitlesByType |
Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute |
Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute |
Gets a time attribute by Title and array Index. |
GetIntegerAttribute |
Gets an integer attribute by title. |
GetIntegerUserAttribute |
Gets an integer attribute by Title and array Index. |
GetMachiningFeatures |
Get the Machining Features |
GetNextUserAttribute |
Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue |
Gets the value of PDM Reference attribute for given object. |
GetProduct |
Get the Product |
GetRealAttribute |
Gets a real attribute by title. |
GetRealUserAttribute |
Gets a real attribute by Title and array Index. |
GetReferenceAttribute |
Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSetup |
Get the Setup |
GetStringAttribute |
Gets a string attribute value by title. |
GetStringUserAttribute |
Gets a string attribute by Title and array Index. |
GetTimeAttribute |
Gets a time attribute by title. |
GetTimeUserAttribute |
Gets a time attribute by Title and array Index. |
GetUserAttribute |
Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString |
Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount |
Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock |
Determine the lock of the given attribute. |
GetUserAttributeSize |
Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects |
Returns an array of objects from which this object presents attributes. |
GetUserAttributes |
Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings |
Gets all the attributes that have been set on the given object. |
HasUserAttribute |
Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight |
Highlights the object. |
Print |
Prints a representation of this object to the system log file. |
RedisplayObject |
Redisplays the object in all views. |
RemoveViewDependency |
Remove dependency on all views from an object. |
SetAttribute |
Creates or modifies an integer attribute. |
SetBooleanUserAttribute |
Creates or modifies a boolean attribute with the option to update or not. |
SetName |
Sets the custom name of the object. |
SetNameLocation |
Sets the location of the object’s name. |
SetPdmReferenceAttribute |
Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute |
Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute |
Creates or modifies a time attribute. |
SetTimeUserAttribute |
Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute |
Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock |
Lock or unlock the given attribute. |
Unblank |
Unblanks the object. |
Unhighlight |
Unhighlights the object. |