SpringDamperCollection Class¶
-
class
NXOpen.Mechatronics.
SpringDamperCollection
¶ Bases:
object
Represents a collection of Spring Damper.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateSpringDamperBuilder | Creates a NXOpen.Mechatronics.SpringDamperBuilder . |
FindObject | Finds the NXOpen.Mechatronics.SpringDamper with the given name. |
Method Detail¶
CreateSpringDamperBuilder¶
-
SpringDamperCollection.
CreateSpringDamperBuilder
¶ Creates a
NXOpen.Mechatronics.SpringDamperBuilder
.Signature
CreateSpringDamperBuilder(springDamper)
Parameters: springDamper ( NXOpen.Mechatronics.SpringDamper
) –NXOpen.Mechatronics.SpringDamper
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.SpringDamperBuilder
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
SpringDamperCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.SpringDamper
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.SpringDamper
.Returns: NXOpen.Mechatronics.SpringDamper
with this name.Return type: NXOpen.Mechatronics.SpringDamper
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)