SpringDamperBuilder Class¶
-
class
NXOpen.Mechatronics.
SpringDamperBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsConstraintBuilder
Represents a
NXOpen.Mechatronics.SpringDamper
builder.To create a new instance of this class, use
NXOpen.Mechatronics.SpringDamperCollection.CreateSpringDamperBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
AxisJoint | Returns the joint select. |
AxisType | Returns or sets the axis joint type. |
Damping | Returns the damping. |
Name | Returns or sets the name. |
RelaxedPosition | Returns the relaxed position. |
SpringConstant | Returns the spring constant. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SpringDamperBuilderAxisJointType Enumeration | the Axis Joint types. |
Property Detail¶
AxisJoint¶
-
SpringDamperBuilder.
AxisJoint
¶ Returns the joint select.
This can be a
NXOpen.Mechatronics.HingeJoint
,NXOpen.Mechatronics.SlidingJoint
andNXOpen.Mechatronics.CylindricalJoint
.-------------------------------------
Getter Method
Signature
AxisJoint
Returns: Return type: NXOpen.Mechatronics.SelectPhysicsJoint
New in version NX10.0.0.
License requirements: None.
AxisType¶
-
SpringDamperBuilder.
AxisType
¶ Returns or sets the axis joint type.
-------------------------------------
Getter Method
Signature
AxisType
Returns: Return type: NXOpen.Mechatronics.SpringDamperBuilderAxisJointType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisType
Parameters: axisType ( NXOpen.Mechatronics.SpringDamperBuilderAxisJointType
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Damping¶
-
SpringDamperBuilder.
Damping
¶ Returns the damping.
-------------------------------------
Getter Method
Signature
Damping
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RelaxedPosition¶
-
SpringDamperBuilder.
RelaxedPosition
¶ Returns the relaxed position.
-------------------------------------
Getter Method
Signature
RelaxedPosition
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SpringConstant¶
-
SpringDamperBuilder.
SpringConstant
¶ Returns the spring constant.
-------------------------------------
Getter Method
Signature
SpringConstant
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
SpringDamperBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.