ScrewJointBuilder Class¶
-
class
NXOpen.Mechatronics.
ScrewJointBuilder
¶ Bases:
NXOpen.Mechatronics.PhysicsJointBuilder
Represents a
NXOpen.Mechatronics.ScrewJoint
builder.To create a new instance of this class, use
NXOpen.Mechatronics.ScrewJointCollection.CreateScrewJointBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
Attachment | Returns the attachment of joint. |
AxisVector | Returns or sets a value that specifies axis vector. |
Base | Returns the base of joint. |
BaseAnchorPoint | Returns or sets the anchor point of base. |
BaseAxisVector | Returns or sets the axis vector of base. |
ExpressionRatio | Returns a value that indicates ratio value for the screw joint. |
Name | Returns or sets the name. |
PointOrigin | Returns or sets a value that indicates the origin point. |
Positioning | Returns or sets a boolean value that indicates whether to create an assembly joint. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AxisVector¶
-
ScrewJointBuilder.
AxisVector
¶ Returns or sets a value that specifies axis vector.
-------------------------------------
Getter Method
Signature
AxisVector
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
AxisVector
Parameters: axisVector ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ExpressionRatio¶
-
ScrewJointBuilder.
ExpressionRatio
¶ Returns a value that indicates ratio value for the screw joint.
-------------------------------------
Getter Method
Signature
ExpressionRatio
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
PointOrigin¶
-
ScrewJointBuilder.
PointOrigin
¶ Returns or sets a value that indicates the origin point.
-------------------------------------
Getter Method
Signature
PointOrigin
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
PointOrigin
Parameters: origin ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
ScrewJointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.