PhysicsJointBuilder Class¶
-
class
NXOpen.Mechatronics.
PhysicsJointBuilder
¶ Bases:
NXOpen.Builder
Represents a base builder for Physics Joints.
This is an abstract class, and cannot be created.
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
Attachment | Returns the attachment of joint. |
Base | Returns the base of joint. |
BaseAnchorPoint | Returns or sets the anchor point of base. |
BaseAxisVector | Returns or sets the axis vector of base. |
Name | Returns or sets the name. |
Positioning | Returns or sets a boolean value that indicates whether to create an assembly joint. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttachment | Sets the attachment. |
SetBase | Sets the base. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Attachment¶
-
PhysicsJointBuilder.
Attachment
¶ Returns the attachment of joint.
This can be a
NXOpen.Mechatronics.RigidBody
or objects which can create a rigid body by.-------------------------------------
Getter Method
Signature
Attachment
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Base¶
-
PhysicsJointBuilder.
Base
¶ Returns the base of joint.
This can be a
NXOpen.Mechatronics.RigidBody
or objects which can create a rigid body by.-------------------------------------
Getter Method
Signature
Base
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
BaseAnchorPoint¶
-
PhysicsJointBuilder.
BaseAnchorPoint
¶ Returns or sets the anchor point of base.
-------------------------------------
Getter Method
Signature
BaseAnchorPoint
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
BaseAnchorPoint
Parameters: point ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
BaseAxisVector¶
-
PhysicsJointBuilder.
BaseAxisVector
¶ Returns or sets the axis vector of base.
-------------------------------------
Getter Method
Signature
BaseAxisVector
Returns: Return type: NXOpen.Direction
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
BaseAxisVector
Parameters: axisVector ( NXOpen.Direction
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Name¶
-
PhysicsJointBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Positioning¶
-
PhysicsJointBuilder.
Positioning
¶ Returns or sets a boolean value that indicates whether to create an assembly joint.
-------------------------------------
Getter Method
Signature
Positioning
Returns: Return type: bool New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Positioning
Parameters: usePositioning (bool) – New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetAttachment¶
-
PhysicsJointBuilder.
SetAttachment
¶ Sets the attachment.
Signature
SetAttachment(attachment)
Parameters: attachment ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetBase¶
-
PhysicsJointBuilder.
SetBase
¶ Sets the base.
Signature
SetBase(base)
Parameters: base ( NXOpen.NXObject
) –New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
PhysicsJointBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.