RuntimeBehaviorBuilder Class¶
-
class
NXOpen.Mechatronics.
RuntimeBehaviorBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.RuntimeBehaviorBuilder
.To create a new instance of this class, use
NXOpen.Mechatronics.RuntimeBehaviorCollection.CreateRuntimeBehaviorBuilder()
New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
Name | Returns or sets the name. |
Source | Returns or sets the source. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetPhysicsObject | Sets physics object |
SetReplacementCode | Sets byte code for replacement |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
StoreExecutableCode | Stores executable code for source |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Name¶
-
RuntimeBehaviorBuilder.
Name
¶ Returns or sets the name.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Source¶
-
RuntimeBehaviorBuilder.
Source
¶ Returns or sets the source.
-------------------------------------
Getter Method
Signature
Source
Returns: Return type: str New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Source
Parameters: source (str) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
SetPhysicsObject¶
-
RuntimeBehaviorBuilder.
SetPhysicsObject
¶ Sets physics object
Signature
SetPhysicsObject(className, propIndex, physicsObject)
Parameters: - className (str) –
- propIndex (int) –
- physicsObject (
NXOpen.NXObject
) –
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetReplacementCode¶
-
RuntimeBehaviorBuilder.
SetReplacementCode
¶ Sets byte code for replacement
Signature
SetReplacementCode(physicsObject)
Parameters: physicsObject ( NXOpen.NXObject
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StoreExecutableCode¶
-
RuntimeBehaviorBuilder.
StoreExecutableCode
¶ Stores executable code for source
Signature
StoreExecutableCode(fileSpec, source)
Parameters: - fileSpec (str) – The file specification
- source (str) – The runtime behavior code
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
RuntimeBehaviorBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.