ReplacePhysicsBuilder Class¶
-
class
NXOpen.Mechatronics.
ReplacePhysicsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ReplacePhysicsBuilder
builder.This class migrates physics objects from replaced component to replacement component in MCD environment, and regeneration of every physics object is done by its own JA interface. To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsManager.CreateReplacePhysicsBuilder()
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
MappingNewphysicsFileid | Maps new physics file id according to the original file id |
MappingNewphysicsObject | Maps new physics object according to the original file id |
ScanPhysicsObject | Scans physics objects in context |
SetReplacementStatus | Set the replacement status |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
MappingNewphysicsFileid¶
-
ReplacePhysicsBuilder.
MappingNewphysicsFileid
¶ Maps new physics file id according to the original file id
Signature
MappingNewphysicsFileid(originalPhysicsObjectPrototypeFileId, newFileId)
Parameters: - originalPhysicsObjectPrototypeFileId (str) – The original physics object file id
- newFileId (str) – The new file id
New in version NX8.5.0.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.ReplacePhysicsBuilder.MappingNewphysicsObject()
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MappingNewphysicsObject¶
-
ReplacePhysicsBuilder.
MappingNewphysicsObject
¶ Maps new physics object according to the original file id
Signature
MappingNewphysicsObject(originalPhysicsObjectPrototypeFileId, newPhysicsObj)
Parameters: - originalPhysicsObjectPrototypeFileId (str) – The original physics object file id
- newPhysicsObj (
NXOpen.NXObject
) – The new physics object to replace
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ScanPhysicsObject¶
-
ReplacePhysicsBuilder.
ScanPhysicsObject
¶ Scans physics objects in context
Signature
ScanPhysicsObject(replacedPartOcc)
Parameters: replacedPartOcc ( NXOpen.Assemblies.Component
) – The replaced part occurenceNew in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SetReplacementStatus¶
-
ReplacePhysicsBuilder.
SetReplacementStatus
¶ Set the replacement status
Signature
SetReplacementStatus(status)
Parameters: status (bool) – The replacement status New in version NX8.5.2.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Validate¶
-
ReplacePhysicsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.