RackPinionCollection Class¶
-
class
NXOpen.Mechatronics.
RackPinionCollection
¶ Bases:
object
Represents a collection of RackPinion.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateRackPinionBuilder | Creates a NXOpen.Mechatronics.RackPinionBuilder . |
FindObject | Finds the NXOpen.Mechatronics.RackPinion with the given name. |
Method Detail¶
CreateRackPinionBuilder¶
-
RackPinionCollection.
CreateRackPinionBuilder
¶ Creates a
NXOpen.Mechatronics.RackPinionBuilder
.Signature
CreateRackPinionBuilder(rackPinion)
Parameters: rackPinion ( NXOpen.Mechatronics.RackPinion
) –NXOpen.Mechatronics.RackPinion
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.RackPinionBuilder
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
RackPinionCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.RackPinion
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.RackPinion
.Returns: NXOpen.Mechatronics.RackPinion
with this name.Return type: NXOpen.Mechatronics.RackPinion
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)