RackPinionBuilder Class¶
-
class
NXOpen.Mechatronics.
RackPinionBuilder
¶ Bases:
NXOpen.Mechatronics.CouplingBuilder
Represents a
Mechatronics.RackPinion
builderTo create a new instance of this class, use
NXOpen.Mechatronics.RackPinionCollection.CreateRackPinionBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AllowSlip | Returns or sets the coulping can slip or not. |
ContactPoint | Returns or sets a value that indicates the contact point value. |
MasterAxisJoint | Returns the master axis joint. |
Name | Returns or sets the name. |
Radius | Returns a value that indicates radius value for the pinion. |
SlaveAxisJoint | Returns the slave axis joint. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetMasterAxisJoint | Sets the master axis. |
SetSlaveAxisJoint | Sets the slave axis. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ContactPoint¶
-
RackPinionBuilder.
ContactPoint
¶ Returns or sets a value that indicates the contact point value.
-------------------------------------
Getter Method
Signature
ContactPoint
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContactPoint
Parameters: contactPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Radius¶
-
RackPinionBuilder.
Radius
¶ Returns a value that indicates radius value for the pinion.
-------------------------------------
Getter Method
Signature
Radius
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
RackPinionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.