ProxyObjectCollection Class¶
-
class
NXOpen.Mechatronics.
ProxyObjectCollection
¶ Bases:
object
Represents a collection of Proxy Object.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateProxyObjectBuilder | Creates a NXOpen.Mechatronics.ProxyObjectBuilder . |
CreateProxyObjectParameterBuilder | Creates a NXOpen.Mechatronics.ProxyObjectParameterBuilder |
FindObject | Finds the NXOpen.Mechatronics.ProxyObject with the given name. |
Method Detail¶
CreateProxyObjectBuilder¶
-
ProxyObjectCollection.
CreateProxyObjectBuilder
¶ Creates a
NXOpen.Mechatronics.ProxyObjectBuilder
.Signature
CreateProxyObjectBuilder(proxyObject)
Parameters: proxyObject ( NXOpen.Mechatronics.ProxyObject
) –NXOpen.Mechatronics.ProxyObject
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ProxyObjectBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateProxyObjectParameterBuilder¶
-
ProxyObjectCollection.
CreateProxyObjectParameterBuilder
¶ Creates a
NXOpen.Mechatronics.ProxyObjectParameterBuilder
Signature
CreateProxyObjectParameterBuilder()
Returns: Return type: NXOpen.Mechatronics.ProxyObjectParameterBuilder
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ProxyObjectCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ProxyObject
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ProxyObject
.Returns: NXOpen.Mechatronics.ProxyObject
with this name.Return type: NXOpen.Mechatronics.ProxyObject
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)