ProxyObjectBuilder Class¶
-
class
NXOpen.Mechatronics.
ProxyObjectBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.ProxyObjectBuilder
.To create a new instance of this class, use
NXOpen.Mechatronics.ProxyObjectCollection.CreateProxyObjectBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
BuilderType | Returns or sets the use type of this builder. |
Context | Returns or sets the context part of the proxy object |
MaxParamId | Returns or sets the maximum parameter id used in the proxy object |
ParameterList | Returns the parameter data |
ProxyObjectName | Returns or sets the name of the proxy object |
SelectGeomObject | Returns the select geometry object that describes the proxy object |
SelectPhysicsObject | Returns the select physics objects that are encapsulated in the proxy object |
Tag | Returns the Tag for this object. |
UseType | Returns or sets the use type used in the proxy object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProxyObjectBuilderType Enumeration | the Builder types. |
Property Detail¶
BuilderType¶
-
ProxyObjectBuilder.
BuilderType
¶ Returns or sets the use type of this builder.
-------------------------------------
Getter Method
Signature
BuilderType
Returns: Return type: NXOpen.Mechatronics.ProxyObjectBuilderType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
BuilderType
Parameters: useType ( NXOpen.Mechatronics.ProxyObjectBuilderType
) –New in version NX9.0.2.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Context¶
-
ProxyObjectBuilder.
Context
¶ Returns or sets the context part of the proxy object
-------------------------------------
Getter Method
Signature
Context
Returns: Return type: NXOpen.BasePart
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Context
Parameters: context ( NXOpen.BasePart
) –New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MaxParamId¶
-
ProxyObjectBuilder.
MaxParamId
¶ Returns or sets the maximum parameter id used in the proxy object
-------------------------------------
Getter Method
Signature
MaxParamId
Returns: Return type: int New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MaxParamId
Parameters: paramId (int) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ParameterList¶
-
ProxyObjectBuilder.
ParameterList
¶ Returns the parameter data
-------------------------------------
Getter Method
Signature
ParameterList
Returns: Return type: NXOpen.Mechatronics.ProxyObjectParameterBuilderList
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ProxyObjectName¶
-
ProxyObjectBuilder.
ProxyObjectName
¶ Returns or sets the name of the proxy object
-------------------------------------
Getter Method
Signature
ProxyObjectName
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ProxyObjectName
Parameters: proxyObjectName (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SelectGeomObject¶
-
ProxyObjectBuilder.
SelectGeomObject
¶ Returns the select geometry object that describes the proxy object
-------------------------------------
Getter Method
Signature
SelectGeomObject
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SelectPhysicsObject¶
-
ProxyObjectBuilder.
SelectPhysicsObject
¶ Returns the select physics objects that are encapsulated in the proxy object
-------------------------------------
Getter Method
Signature
SelectPhysicsObject
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
UseType¶
-
ProxyObjectBuilder.
UseType
¶ Returns or sets the use type used in the proxy object.
Use
NXOpen.Mechatronics.ProxyObjectBuilder.BuilderType`()
instead.-------------------------------------
Getter Method
Signature
UseType
Returns: Return type: int New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
UseType
Parameters: useType (int) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
ProxyObjectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.