PreferencesBuilder Class¶
-
class
NXOpen.Mechatronics.
PreferencesBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Mechatronics.PreferencesBuilder
builder.To create a new instance of this class, use
NXOpen.Mechatronics.PhysicsPreferenceCollection.CreatePreferenceBuilder()
Default values.
Property Value AngularDampingExpression.Value 3490.6585 (millimeters part), 0.030895 (inches part) CoSimulation false CollisionPrecisionExpression.Value 0.1 (millimeters part), 0.0039 (inches part) ConnectURL DynamicFrictionExpression.Value 0.7 EnablePlcSimAdvTimeSyn false EnableTimeSync false ErrorReductionExpression.Value 50 Gx.Value 0 (millimeters part), 0 (inches part) Gy.Value 0 (millimeters part), 0 (inches part) Gz.Value -9806.65 (millimeters part), -386.09 (inches part) LinearDampingExpression.Value 0.05 (millimeters part), 0.0002855 (inches part) MaxIterationExpression.Value 100 RestitutionExpression.Value 0.01 RollingFrictionExpression.Value 0.0 SpringForceMultiplierExpression.Value 100 StaticFrictionExpression.Value 0.7 StepTimeExpression.Value 0.001 ToleranceExpression.Value 0.1 (millimeters part), 0.0039 (inches part) New in version NX7.5.1.
Properties¶
Property | Description |
---|---|
AngularDampingExpression | Returns the angular damping expression |
CoSimulation | Returns or sets the co-simulation option |
CollisionPrecision | Returns or sets the collision precision. |
CollisionPrecisionExpression | Returns the Collision Precision Expression |
ConnectURL | Returns or sets the Simit Connect URL string |
DynamicFriction | Returns or sets the dynamic friction. |
DynamicFrictionExpression | Returns the Dynamic Friction Expression |
EnablePlcSimAdvTimeSyn | Returns or sets the plcsim adv time synchronization option |
EnableTimeSync | Returns or sets the time synchronization option |
ErrorReduction | Returns or sets the error reduction. |
ErrorReductionExpression | Returns the Error Reduction Expression |
FilePicker | Returns or sets the export timing chart file path |
ForwardStepTime | Returns the Forward Step Time Expression |
GeometryHighlight | Returns or sets the geometry highlight on collsion. |
Gx | Returns the gx. |
Gy | Returns the gy. |
Gz | Returns the gz. |
InvokeExport | Returns or sets the toggle value for the invoke timing chart after import |
LinearDampingExpression | Returns the linear damping expression |
LoadAsSaved | Returns or sets the load as saved option for MCD Objects. |
MasterType | Returns or sets the master type option |
MaxIteration | Returns or sets the max iteration. |
MaxIterationExpression | Returns the Maximum Iteration Expression |
RefreshPrecision | Returns or sets the inspector refresh precision. |
Restitution | Returns or sets the restitution. |
RestitutionExpression | Returns the Restitution Expression |
RevisionRule | Returns or sets the revision rule for MCD Objects. |
RollingFrictionExpression | Returns the rolling Friction Expression |
ShapeHighlight | Returns or sets the shape highlight on collsion. |
SpringForceMultiplier | Returns or sets the spring force multiplier. |
SpringForceMultiplierExpression | Returns the Spring Force Multiplier Expression |
StaticFriction | Returns or sets the static friction. |
StaticFrictionExpression | Returns the static Friction Expression |
StepSize | Returns the Step Size Expression |
StepTime | Returns or sets the step time. |
StepTimeExpression | Returns the Step Time Expression |
StickyFactor | Returns or sets the sticky factor. |
StickyForce | Returns the sticky factor Expression |
SynchronizationTime | Returns the time interval to do synchronization with SIMIT |
Tag | Returns the Tag for this object. |
TimeScaleFactor | Returns or sets the time scale factor |
Tolerance | Returns or sets the tolerance. |
ToleranceExpression | Returns the Tolerance Expression |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PreferencesBuilderMasterTypes Enumeration | the Co-Simulation master type. |
Property Detail¶
AngularDampingExpression¶
-
PreferencesBuilder.
AngularDampingExpression
¶ Returns the angular damping expression
-------------------------------------
Getter Method
Signature
AngularDampingExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CoSimulation¶
-
PreferencesBuilder.
CoSimulation
¶ Returns or sets the co-simulation option
-------------------------------------
Getter Method
Signature
CoSimulation
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
CoSimulation
Parameters: coSimulation (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CollisionPrecision¶
-
PreferencesBuilder.
CollisionPrecision
¶ Returns or sets the collision precision.
-------------------------------------
Getter Method
Signature
CollisionPrecision
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.CollisionPrecisionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
CollisionPrecision
Parameters: collisionPrecision (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CollisionPrecisionExpression¶
-
PreferencesBuilder.
CollisionPrecisionExpression
¶ Returns the Collision Precision Expression
-------------------------------------
Getter Method
Signature
CollisionPrecisionExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ConnectURL¶
-
PreferencesBuilder.
ConnectURL
¶ Returns or sets the Simit Connect URL string
-------------------------------------
Getter Method
Signature
ConnectURL
Returns: Return type: str New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ConnectURL
Parameters: connectURL (str) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DynamicFriction¶
-
PreferencesBuilder.
DynamicFriction
¶ Returns or sets the dynamic friction.
-------------------------------------
Getter Method
Signature
DynamicFriction
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.DynamicFrictionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
DynamicFriction
Parameters: dynamicFriction (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
DynamicFrictionExpression¶
-
PreferencesBuilder.
DynamicFrictionExpression
¶ Returns the Dynamic Friction Expression
-------------------------------------
Getter Method
Signature
DynamicFrictionExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnablePlcSimAdvTimeSyn¶
-
PreferencesBuilder.
EnablePlcSimAdvTimeSyn
¶ Returns or sets the plcsim adv time synchronization option
-------------------------------------
Getter Method
Signature
EnablePlcSimAdvTimeSyn
Returns: Return type: bool New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnablePlcSimAdvTimeSyn
Parameters: enablePlcSimAdvTimeSyn (bool) – New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
EnableTimeSync¶
-
PreferencesBuilder.
EnableTimeSync
¶ Returns or sets the time synchronization option
-------------------------------------
Getter Method
Signature
EnableTimeSync
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
EnableTimeSync
Parameters: enableTimeSync (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ErrorReduction¶
-
PreferencesBuilder.
ErrorReduction
¶ Returns or sets the error reduction.
-------------------------------------
Getter Method
Signature
ErrorReduction
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.ErrorReductionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ErrorReduction
Parameters: errorReduction (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ErrorReductionExpression¶
-
PreferencesBuilder.
ErrorReductionExpression
¶ Returns the Error Reduction Expression
-------------------------------------
Getter Method
Signature
ErrorReductionExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FilePicker¶
-
PreferencesBuilder.
FilePicker
¶ Returns or sets the export timing chart file path
-------------------------------------
Getter Method
Signature
FilePicker
Returns: Return type: str New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
FilePicker
Parameters: exportFile (str) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ForwardStepTime¶
-
PreferencesBuilder.
ForwardStepTime
¶ Returns the Forward Step Time Expression
-------------------------------------
Getter Method
Signature
ForwardStepTime
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
GeometryHighlight¶
-
PreferencesBuilder.
GeometryHighlight
¶ Returns or sets the geometry highlight on collsion.
-------------------------------------
Getter Method
Signature
GeometryHighlight
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
GeometryHighlight
Parameters: highlight (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Gx¶
-
PreferencesBuilder.
Gx
¶ Returns the gx.
-------------------------------------
Getter Method
Signature
Gx
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Gy¶
-
PreferencesBuilder.
Gy
¶ Returns the gy.
-------------------------------------
Getter Method
Signature
Gy
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Gz¶
-
PreferencesBuilder.
Gz
¶ Returns the gz.
-------------------------------------
Getter Method
Signature
Gz
Returns: Return type: NXOpen.Expression
New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
InvokeExport¶
-
PreferencesBuilder.
InvokeExport
¶ Returns or sets the toggle value for the invoke timing chart after import
-------------------------------------
Getter Method
Signature
InvokeExport
Returns: Return type: bool New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
InvokeExport
Parameters: param (bool) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LinearDampingExpression¶
-
PreferencesBuilder.
LinearDampingExpression
¶ Returns the linear damping expression
-------------------------------------
Getter Method
Signature
LinearDampingExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
LoadAsSaved¶
-
PreferencesBuilder.
LoadAsSaved
¶ Returns or sets the load as saved option for MCD Objects.
-------------------------------------
Getter Method
Signature
LoadAsSaved
Returns: Return type: bool New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
LoadAsSaved
Parameters: loadAsSaved (bool) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MasterType¶
-
PreferencesBuilder.
MasterType
¶ Returns or sets the master type option
-------------------------------------
Getter Method
Signature
MasterType
Returns: Return type: NXOpen.Mechatronics.PreferencesBuilderMasterTypes
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MasterType
Parameters: masterType ( NXOpen.Mechatronics.PreferencesBuilderMasterTypes
) –New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MaxIteration¶
-
PreferencesBuilder.
MaxIteration
¶ Returns or sets the max iteration.
-------------------------------------
Getter Method
Signature
MaxIteration
Returns: Return type: int New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.MaxIterationExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
MaxIteration
Parameters: maxIter (int) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
MaxIterationExpression¶
-
PreferencesBuilder.
MaxIterationExpression
¶ Returns the Maximum Iteration Expression
-------------------------------------
Getter Method
Signature
MaxIterationExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RefreshPrecision¶
-
PreferencesBuilder.
RefreshPrecision
¶ Returns or sets the inspector refresh precision.
This option specifies the refresh precision to be used by the inspector to determine whether to update property values in UI or not.
-------------------------------------
Getter Method
Signature
RefreshPrecision
Returns: Return type: float New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
RefreshPrecision
Parameters: refreshPrecision (float) – New in version NX7.5.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Restitution¶
-
PreferencesBuilder.
Restitution
¶ Returns or sets the restitution.
-------------------------------------
Getter Method
Signature
Restitution
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.RestitutionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Restitution
Parameters: restitution (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RestitutionExpression¶
-
PreferencesBuilder.
RestitutionExpression
¶ Returns the Restitution Expression
-------------------------------------
Getter Method
Signature
RestitutionExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RevisionRule¶
-
PreferencesBuilder.
RevisionRule
¶ Returns or sets the revision rule for MCD Objects.
-------------------------------------
Getter Method
Signature
RevisionRule
Returns: Return type: str New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
RevisionRule
Parameters: revisionRule (str) – New in version NX8.5.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
RollingFrictionExpression¶
-
PreferencesBuilder.
RollingFrictionExpression
¶ Returns the rolling Friction Expression
-------------------------------------
Getter Method
Signature
RollingFrictionExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ShapeHighlight¶
-
PreferencesBuilder.
ShapeHighlight
¶ Returns or sets the shape highlight on collsion.
-------------------------------------
Getter Method
Signature
ShapeHighlight
Returns: Return type: bool New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
ShapeHighlight
Parameters: highlight (bool) – New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SpringForceMultiplier¶
-
PreferencesBuilder.
SpringForceMultiplier
¶ Returns or sets the spring force multiplier.
-------------------------------------
Getter Method
Signature
SpringForceMultiplier
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.SpringForceMultiplierExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
SpringForceMultiplier
Parameters: springForceMultiplier (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SpringForceMultiplierExpression¶
-
PreferencesBuilder.
SpringForceMultiplierExpression
¶ Returns the Spring Force Multiplier Expression
-------------------------------------
Getter Method
Signature
SpringForceMultiplierExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StaticFriction¶
-
PreferencesBuilder.
StaticFriction
¶ Returns or sets the static friction.
-------------------------------------
Getter Method
Signature
StaticFriction
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.StaticFrictionExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
StaticFriction
Parameters: staticFriction (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StaticFrictionExpression¶
-
PreferencesBuilder.
StaticFrictionExpression
¶ Returns the static Friction Expression
-------------------------------------
Getter Method
Signature
StaticFrictionExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StepSize¶
-
PreferencesBuilder.
StepSize
¶ Returns the Step Size Expression
-------------------------------------
Getter Method
Signature
StepSize
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StepTime¶
-
PreferencesBuilder.
StepTime
¶ Returns or sets the step time.
-------------------------------------
Getter Method
Signature
StepTime
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.StepTimeExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
StepTime
Parameters: stepTime (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StepTimeExpression¶
-
PreferencesBuilder.
StepTimeExpression
¶ Returns the Step Time Expression
-------------------------------------
Getter Method
Signature
StepTimeExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StickyFactor¶
-
PreferencesBuilder.
StickyFactor
¶ Returns or sets the sticky factor.
-------------------------------------
Getter Method
Signature
StickyFactor
Returns: Return type: float New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.StickyForce()
instead.License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
StickyFactor
Parameters: factor (float) – New in version NX10.0.0.
Deprecated since version NX11.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
StickyForce¶
-
PreferencesBuilder.
StickyForce
¶ Returns the sticky factor Expression
-------------------------------------
Getter Method
Signature
StickyForce
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
SynchronizationTime¶
-
PreferencesBuilder.
SynchronizationTime
¶ Returns the time interval to do synchronization with SIMIT
-------------------------------------
Getter Method
Signature
SynchronizationTime
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
TimeScaleFactor¶
-
PreferencesBuilder.
TimeScaleFactor
¶ Returns or sets the time scale factor
-------------------------------------
Getter Method
Signature
TimeScaleFactor
Returns: Return type: float New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
TimeScaleFactor
Parameters: scaleFactor (float) – New in version NX10.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Tolerance¶
-
PreferencesBuilder.
Tolerance
¶ Returns or sets the tolerance.
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX7.5.1.
Deprecated since version NX9.0.0: Use
NXOpen.Mechatronics.PreferencesBuilder.ToleranceExpression()
insteadLicense requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX7.5.1.
Deprecated since version NX9.0.0: This functionality is no longer supported.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
ToleranceExpression¶
-
PreferencesBuilder.
ToleranceExpression
¶ Returns the Tolerance Expression
-------------------------------------
Getter Method
Signature
ToleranceExpression
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
Method Detail¶
Validate¶
-
PreferencesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.