PhysicsPreferenceCollection Class

class NXOpen.Mechatronics.PhysicsPreferenceCollection

Bases: object

Represents a collection of Physics Preference.

To obtain an instance of this class, refer to NXOpen.Mechatronics.PhysicsManager

New in version NX9.0.0.

Methods

Method Description
CreatePreferenceBuilder Creates a NXOpen.Mechatronics.PreferencesBuilder.
FindObject Finds the NXOpen.Mechatronics.PhysicsPreference with the given name.

Method Detail

CreatePreferenceBuilder

PhysicsPreferenceCollection.CreatePreferenceBuilder

Creates a NXOpen.Mechatronics.PreferencesBuilder.

Signature CreatePreferenceBuilder(physicsPreference)

Parameters:physicsPreference (NXOpen.Mechatronics.PhysicsPreference) – NXOpen.Mechatronics.PhysicsPreference to be edited, if None then create a new one
Returns:
Return type:NXOpen.Mechatronics.PreferencesBuilder

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)

FindObject

PhysicsPreferenceCollection.FindObject

Finds the NXOpen.Mechatronics.PhysicsPreference with the given name.

An exception will be thrown if no object can be found with given name.

Signature FindObject(name)

Parameters:name (str) – The name of the NXOpen.Mechatronics.PhysicsPreference.
Returns:NXOpen.Mechatronics.PhysicsPreference with this name.
Return type:NXOpen.Mechatronics.PhysicsPreference

New in version NX9.0.0.

License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)