ExternalConnectionCollection Class¶
-
class
NXOpen.Mechatronics.
ExternalConnectionCollection
¶ Bases:
object
Represents a collection of External Connection.
To obtain an instance of this class, refer to
NXOpen.Mechatronics.PhysicsManager
New in version NX8.0.0.
Methods¶
Method | Description |
---|---|
CreateExternalConnectionBuilder | Creates a NXOpen.Mechatronics.ExternalConnectionBuilder . |
CreateExternalConnectionElementBuilder | Creates a NXOpen.Mechatronics.ExternalConnectionElementBuilder |
FindObject | Finds the NXOpen.Mechatronics.ExternalConnection with the given name. |
Method Detail¶
CreateExternalConnectionBuilder¶
-
ExternalConnectionCollection.
CreateExternalConnectionBuilder
¶ Creates a
NXOpen.Mechatronics.ExternalConnectionBuilder
.Signature
CreateExternalConnectionBuilder(exteral)
Parameters: exteral ( NXOpen.Mechatronics.ExternalConnection
) –NXOpen.Mechatronics.ExternalConnection
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ExternalConnectionBuilder
New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
CreateExternalConnectionElementBuilder¶
-
ExternalConnectionCollection.
CreateExternalConnectionElementBuilder
¶ Creates a
NXOpen.Mechatronics.ExternalConnectionElementBuilder
Signature
CreateExternalConnectionElementBuilder(element)
Parameters: element ( NXOpen.Mechatronics.ExternalConnectionElement
) –NXOpen.Mechatronics.ExternalConnectionElement
to be edited, if None then create a new oneReturns: Return type: NXOpen.Mechatronics.ExternalConnectionElementBuilder
New in version NX8.0.1.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)
FindObject¶
-
ExternalConnectionCollection.
FindObject
¶ Finds the
NXOpen.Mechatronics.ExternalConnection
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Mechatronics.ExternalConnection
.Returns: NXOpen.Mechatronics.ExternalConnection
with this name.Return type: NXOpen.Mechatronics.ExternalConnection
New in version NX8.0.0.
License requirements: nx_mcd_core (“MECHATRONICS CONCEPT DESIGNER”)